cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F411CEU6 with SMT32Cube.MX, AI & IDE Youtube example build errors.

debugging
Lead

Trying to start with STM32 and AI. Ubuntu 19.04 STM32Cube.MX 5.3.0 with STM32Cube.AI installed. ,STM32CubeMX IDE 1.0.1. Using an STM32F411CEU6 (8x compression). Following this example"Getting Started with STM32Cube.AI" but using the STM32 Toolchain (nt everyone bought IAR) got the following build errors in STM32Cube IDE.

Update #1. Added FREERTOS and in SYS selected Timebase TM1. The CMSIS and tick error are gone but now there are errors as shown in the attached txt file. It seems some constants are not declared Both with FREERTOS CMSIS_v1 and CMSIS_V2. What is missing ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Hopeful Programmer
Associate II

Same problem on my end using the STM32Cube