cancel
Showing results for 
Search instead for 
Did you mean: 

SAI bit clock and FS line become corrupted while using NPU

s319189
Associate III

I’ve generated a project with Cube AI studio for a Nucleo N6 board, but , when I enable SAI2 peripheral in I2S mode, I notice from the oscilloscope that the bit clock line and FS line become corrupted/glitch when using NPU for inference, could somebody explain me why and how to solve it? 
I’ve used the same SAI configuration for another project without any AI algorithm and the signals from the pins are clean. I don’t know why, it’s a problem that I’ve been stuck for a month or so

0 REPLIES 0