2025-10-20 6:12 PM
hi,all.
I used “best_saved_model/best_integer_quant.tflite” to perform inference on the PC,it's looks success!
tflite_model = YOLO("/home/alientek/best_saved_model/best_integer_quant.tflite")
# Run inference
results = tflite_model("/home/alientek/hander1_1.jpg")
and output like this.
(yolov11) alientek@ubuntu:~/yolov11$ python test1.py
/home/alientek/.conda/envs/yolov11/lib/python3.10/site-packages/requests/__init__.py:86: RequestsDependencyWarning: Unable to find acceptable character detection dependency (chardet or charset_normalizer).
warnings.warn(
WARNING ⚠️ Unable to automatically guess model task, assuming 'task=detect'. Explicitly define task for your model, i.e. 'task=detect', 'segment', 'classify','pose' or 'obb'.
Loading /home/alientek/best_saved_model/best_integer_quant.tflite for TensorFlow Lite inference...
INFO: Created TensorFlow Lite XNNPACK delegate for CPU.
image 1/1 /home/alientek/hander1_1.jpg: 640x640 1 handler1, 1760.9ms
Speed: 38.9ms preprocess, 1760.9ms inference, 26.5ms postprocess per image at shape (1, 3, 640, 640)
But when I deploy to the stm32mp257 using the following code, the target is not detected.
for (int w = 0; w < 8400; w++)
{
float cx = data[0 * 8400 + w];
float cy = data[1 * 8400 + w];
float w_box = data[2 * 8400 + w];
float h_box = data[3 * 8400 + w];
// Find class with max probability
float max_score = 0;
int max_class = -1;
for (int c = 0; c < num_classes; c++)
{
float score = data[(4 + c) * 8400 + w];
if (score > max_score)
{
max_score = score;
max_class = c;
}
}
if (max_score > confidence_threshold)
{
ObjDetect_Results det;
det.x = cx;
det.y = cy;
det.w = w_box;
det.h = h_box;
det.class_id = max_class;
det.confidence = max_score;
detections.push_back(det);
}
}
Solved! Go to Solution.
2025-10-27 6:20 AM
I think this question is part of this thread. Please don't duplicate threads.
Re: porting yolov11 model to stm32mp257. - Page 2 - STMicroelectronics Community
Have a good day,
Julian
2025-10-27 6:20 AM
I think this question is part of this thread. Please don't duplicate threads.
Re: porting yolov11 model to stm32mp257. - Page 2 - STMicroelectronics Community
Have a good day,
Julian