cancel
Showing results for 
Search instead for 
Did you mean: 

Memory Error in hsdatalog_to_nanoedge.py when converting ISM330DHCX .dat

jtpgilej
Associate II

Hopefully someone can give me a hint on what I am doing wrong.

I am logging sensor data with the STEVAL-PROTEUS1 board to the PC using the fp-sns-datapro1 project and the cli_example method. When I try to convert the binary .dat to .csv of the ISM330DHCX by using the HS-DL_NanoEdge_Conversion.bat the hsdatalog_to_nanoedge.py script rises and exception at line  102

HSDatalogApp.st_hsdatalog.HSD.HSDatalog_v1 - ERROR - Memory Error occoured! You should batch process your ...

It also crashes when converting IIS3DWB .dat, but data logged from IIS2DLPC and SST22H sensors are converted correctly.

I have also tried to convert the example samples provided in directory STM32CubeFunctionPack_DATAPRO1_v1.1.0\Utilities\SwUtilities\HS_Datalog\PROTEUS_batch_file_examples\AcquisitionExample and the same behaviour occurs.

I am using python 3.8 and fp-sns-datapro1 version 1.1

.dat collected by bluetooth via STSBLESens App or by USB in MSD mode have also the same problem.

Best regards

0 REPLIES 0