2025-03-10 9:04 AM
This is the error i get when trying to clone the git.
C:\Users\Zhun>git clone https://github.com/STMicroelectronics/stm32ai-modelzoo.git
Cloning into 'stm32ai-modelzoo'...
remote: Enumerating objects: 8704, done.
remote: Counting objects: 100% (348/348), done.
remote: Compressing objects: 100% (82/82), done.
error: RPC failed; curl 92 HTTP/2 stream 5 was not closed cleanly: CANCEL (err 8)
error: 5254 bytes of body are still expected
fetch-pack: unexpected disconnect while reading sideband packet
fatal: early EOF
fatal: fetch-pack: invalid index-pack output
2025-03-11 1:30 AM
Hello @jzzunn ,
Can you try to follow the Before you Start first:
STMicroelectronics/stm32ai-modelzoo: AI Model Zoo for STM32 devices
Please tell me if it solve your issue.
Also note that ST Model Zoo is splitted in two distinct repositories:
The first one contains only models, where the second one contains all the scripts to train, quantize, ..., deploy a model.
Have a good day,
Julian