cancel
Showing results for 
Search instead for 
Did you mean: 

Error deploying deeplab_v3_mobilenetv2_05_16_320_asppv2_qdq_int8.onnx to STM32N6570-DK.

dev8
Associate

Hi @everyone, 

I’m deploying an AI model on the STM32N6570-DK. The deployment process seems fine — in the command line I see the message:

“Your model deployed. Turn both boot switches to the left and cycle the power.”

However, the issue is that the model is not building in cmd and as well as on STM32CubeIDE. I’ve tried this with 5–10 different models, but every time I get a model build failed error, and the .bin file is not generated.

Any help or suggestions would be greatly appreciated!
Thanks in advance! 


Details:

  • Board: STM32N6570-DK

  • Tools: STM32CubeIDE, STM32Cube.AI, STM32CubeProgrammer.

 

0 REPLIES 0