2022-01-03 6:39 AM
I'm trying to build a .npz file with multiple input and output data.
I achieved to add just one input and output using this code:
np.savez('STM32TestData.npz',
m_inputs_1=input_1,
m_outputs_1=output_1,
)
This works fine, but just one pair of data.Adding more keys as 'm_inputs_2', 'm_outputs_2' didn't worked.
np.savez('STM32TestData.npz',
m_inputs_1=input_1,
m_outputs_1=output_1,
m_inputs_2=input_2,
m_outputs_2=output_2,
)
E204(ValParamError): number of input arrays is invalid, 2 instead 1Also I tried to save data as dictionaries with keys 'm_inputs_idx', 'm_outputs_idx' with 'idx' from 1 to N, but the same error occurred.
np.savez('STM32TestData.npz', **inputs_dict, **outputs_dict)
E204(ValParamError): number of input arrays is invalid, 439 instead 1What is the correct way to do it?
Additionally, what does 'c_inputs_<idx> and c_outputs_<idx> (multiple IO, if no m_inputs_<idx> keys are defined)' mean? How is it different from using 'm' version?
Solved! Go to Solution.
2022-01-03 7:05 AM
Hi @ASalc.1 ,
I had this usecase few weeks ago. I had a model with 1 input and 2 outputs, the correct way to handle it is to start from 0 index:
np.savez('data_io.npz', m_inputs_0=X, m_outputs_0=out_0, m_outputs_1=out_1)"m_inputs/outputs_xx" are inputs/outputs related to the initial model execution
"c_inputs/outputs_xx" are related to inputs and outputs from the C (stm.ai converted) model execution (Can be executed on STM32 or locally on desktop).
Best regards,
Romain
2022-01-03 7:05 AM
Hi @ASalc.1 ,
I had this usecase few weeks ago. I had a model with 1 input and 2 outputs, the correct way to handle it is to start from 0 index:
np.savez('data_io.npz', m_inputs_0=X, m_outputs_0=out_0, m_outputs_1=out_1)"m_inputs/outputs_xx" are inputs/outputs related to the initial model execution
"c_inputs/outputs_xx" are related to inputs and outputs from the C (stm.ai converted) model execution (Can be executed on STM32 or locally on desktop).
Best regards,
Romain
2022-01-03 7:32 AM
Hi Romain, thanks for the answer, it solved my questions!.