cancel
Showing results for 
Search instead for 
Did you mean: 

error while analyzing a neural network (Tflite model) in stm32 cube ai

Luca4
Associate II

good morning, I'm trying to import a neural network for NILM (non-intrusive load monitoring) in the stm32 environment, but I can't complete the analysis due to the presence of the error: 

INTERNAL ERROR: unpack_from requires a buffer of at least 122836864 bytes for unpacking 4 bytes at offset 122836860 (actual buffer size is 1654784)

 The network is CNN type and I'm working with xcube ai v. 9.0.0 and stm32cubeide 1.15.1

I'm asking anyone if they know how I can solve the problem of the buffer size, thanks in advance.

1 ACCEPTED SOLUTION

Accepted Solutions

Thanks for sharing this network, there seem to be something wrong with the generated tflite, I can't open it with Netron, nor with tflite micro and as you saw CubeAI is also reporting an error.

I tried also to dump it in json using flatc but this is producing an error too.

If you have your original model in Keras, we can support it directly in the tool, or I recommend to try to regenerate the tflite from your source.

Regards

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
fauvarque.daniel
ST Employee

Can you share the model please (it can be with random weights)

Regards

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Good morning, this is the neural network that I tried to import, thanks for your answer.

https://drive.google.com/file/d/1VTm0BNQ8uM_mkBeo8TVoX1i1VdZ-GbL2/view?usp=drive_link 

fauvarque.daniel
ST Employee

for this model I have a different error

 

stedgeai analyze --target stm32 -m STUDENT_converted_model.tflite
STEdgeAI Core v9.0.0-19802

NOT IMPLEMENTED: Unsupported layer types: FlexTensorListReserve, FlexTensorListS
tack, WHILE, stopping.

As  of today we support RNN only in float keras format.

The conversion in TFLite is introducing layers that we don't support for the moment (for example While)

Regards

Daniel

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Luca4
Associate II

Sorry, my mistake, the network I shared before was an old version of the one I need (that was with a CRNN approach), below I'll send you the one that gives me the type of error I was talking about in the first post

https://drive.google.com/file/d/1FhDdYCNd0y86SptZ5FHCSjpUQdkdxXZ9/view?usp=drive_link

Thanks for sharing this network, there seem to be something wrong with the generated tflite, I can't open it with Netron, nor with tflite micro and as you saw CubeAI is also reporting an error.

I tried also to dump it in json using flatc but this is producing an error too.

If you have your original model in Keras, we can support it directly in the tool, or I recommend to try to regenerate the tflite from your source.

Regards

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.