2024-12-12 4:48 AM
As stated, I have problem analyzing the ONNX model ported from a pytorch model. The code of the model is simple as follows:
class LSTM(nn.Module):
def __init__(self, input_size, hidden_size, num_layers, num_output=1):
super(LSTM, self).__init__()
self.num_layers = num_layers
self.input_size = input_size
self.hidden_size = hidden_size
self.num_output = num_output
self.lstm = nn.LSTM(input_size=input_size, hidden_size=hidden_size,
num_layers=num_layers, batch_first=True)
self.fc = nn.Linear(hidden_size, num_output)
def forward(self, x, device='cuda'):
ula, (h_out, _) = self.lstm(x)
out = self.fc(h_out[-1])
return out
Netron vis:
I will really appreciate any advice or workarounds. Thank you!
Solved! Go to Solution.
2024-12-18 7:31 AM
Thank you very much!
2024-12-20 1:10 AM
Hello @Lemanoise,
I should know more about how to use LSTM properly with ST Edge AI Core on the start of next year.
But for the moment I managed to use more than one hidden size with pytorch by not using the batch_first option:
import torch
import torch.nn as nn
class LSTM(nn.Module):
def __init__(self, input_size, hidden_size, num_layers, num_output=1):
super(LSTM, self).__init__()
self.num_layers = num_layers
self.input_size = input_size
self.hidden_size = hidden_size
self.num_output = num_output
self.lstm = nn.LSTM(input_size=input_size, hidden_size=hidden_size,
num_layers=num_layers, batch_first=False)
self.fc = nn.Linear(hidden_size, num_output)
def forward(self, x, device='cuda'):
ula, (h_out, _) = self.lstm(x)
out = self.fc(h_out[-1])
return out
# If not 1 : error
# other we can put anything
input_size = 10
hidden_size = 10
num_layers = 1
num_output = 10
model = LSTM(input_size, hidden_size, num_layers, num_output)
model.eval()
dummy_input = torch.randn(1, 128, input_size) # Batch size 1, Sequence length 128, Input size 10
onnx_file_path = "simple_lstml.onnx"
torch.onnx.export(model, dummy_input, onnx_file_path,
input_names=['input'], output_names=['output'])
It may help you
Have a good day,
Julian