Skip to main content
Visitor II
February 28, 2025
Question

cube-ai

  • February 28, 2025
  • 1 reply
  • 1058 views

masirwlw_0-1740736241654.png

 

 

#undef __FPU_PRESENT
#include "stm32h7xx.h"
#include "main.h"
#include "crc.h"
#include "memorymap.h"
#include "gpio.h"
#include "app_x-cube-ai.h"
#include "network.h"
#include "ai_platform.h"
#include "network_data.h"
#include <stdlib.h>
#include <stdio.h>
#include "network_data.h" // 确保包含权重数据声明



/* 手动定义缺失的宏(必须与network.c中的实际值一致) */
#ifndef AI_NETWORK_WEIGHTS_SIZE
#define AI_NETWORK_WEIGHTS_SIZE 794136 // 根据network.c中的值填写
#endif

#ifndef AI_NETWORK_ACTIVATIONS_SIZE
#define AI_NETWORK_ACTIVATIONS_SIZE 45572 // 根据network.c中的值填写
#endif

/* 输入输出缓冲区定义 */
AI_ALIGNED(32) static float input_data[90 * 3 * 1 * 1] = {0}; // 严格匹配network.c输入形状
AI_ALIGNED(32) static float output_data[1 * 1 * 6 * 1] = {0}; // 匹配输出形状



static ai_handle network_handle = AI_HANDLE_NULL;


/* 函数原型声明 -------------------------------------------------------------*/
void SystemClock_Config(void);
static void MPU_Config(void);
static int argmax(const float *arr, int size);
void Error_Handler(void);

int main(void)
{

 MPU_Config();
 HAL_Init();
 SystemClock_Config();
 MX_GPIO_Init();
 MX_CRC_Init();
 MX_Core_Init();
 printf("AI Model Initialized\n");
 
 /* 1. 创建网络实例 */
 ai_error err = ai_mnetwork_create(
 AI_NETWORK_MODEL_NAME, // 使用network.h中定义的模型名称
 &network_handle,
 NULL // 使用默认配置
 );
 
 if (err.type != AI_ERROR_NONE) {
 printf("Network create error: 0x%08X\n", err.code);
 Error_Handler();
 }

 printf("1\n");
 
 
 /* 2. 初始化网络参数 */
 ai_network_params params = {
 .params = {
 .format = AI_BUFFER_FORMAT_U8,
 .n_batches = 1,
 .height = 1,
 .width = AI_NETWORK_WEIGHTS_SIZE,
 .channels = 1,
 .data = AI_HANDLE_PTR(ai_network_data_weights_get())
 },
 .activations = {
 .format = AI_BUFFER_FORMAT_U8,
 .n_batches = 1,
 .height = 1,
 .width = AI_NETWORK_ACTIVATIONS_SIZE,
 .channels = 1,
 .data = AI_HANDLE_PTR(input_data)
 }
 };

 if (!ai_mnetwork_init(network_handle, &params)) {
 printf("Network init failed\n");
 ai_mnetwork_destroy(network_handle);
 Error_Handler();
 }
 
 printf("2\n");
 
 /* 3. 配置输入输出缓冲区 */
 ai_buffer input_buf = AI_BUFFER_OBJ_INIT(
 AI_BUFFER_FORMAT_FLOAT, // format_
 90, // height (根据network.c中的AI_SHAPE_INIT(90,3,1,1))
 3, // width
 1, // channels
 1, // n_batches
 input_data // data
 );

 ai_buffer output_buf = AI_BUFFER_OBJ_INIT(
 AI_BUFFER_FORMAT_FLOAT,
 1, // height (根据network.c中的AI_SHAPE_INIT(1,1,6,1))
 1,
 6,
 1,
 output_data
 );
 
 /* 主循环 */
 srand(HAL_GetTick());
 
 printf("3\n");
 
 while (1)
 {
 /* 生成输入数据 */
 for (int i = 0; i < 90 * 3; i++) {
 input_data[i] = (2.0f * rand() / RAND_MAX) - 1.0f;
 }
 printf("4\n");
 /* 缓存维护 */
 SCB_CleanDCache_by_Addr(
 (uint32_t*)((uintptr_t)input_data & ~0x1F),
 sizeof(input_data) + 32
 );

 // 在调用前添加地址验证
printf("ai_network_run实际地址: 0x%08X\n", (uint32_t)ai_network_run);
 
 

 
 
 /* 执行推理 */
 int result = ai_mnetwork_run(network_handle, &input_buf, &output_buf);
 
 if (result != AI_ERROR_NONE) {
 printf("Inference error: %d\n", result);
 Error_Handler();
 }

 /* 处理输出 */
 SCB_InvalidateDCache_by_Addr(
 (uint32_t*)((uintptr_t)output_data & ~0x1F),
 sizeof(output_data) + 32
 );

 int class_id = argmax(output_data, 6);
 printf("Predicted class: %d\n", class_id);
 HAL_Delay(1000);
 }
 

}



/* 实现必须严格匹配声明 */
static int argmax(const float *arr, int size)
{
 int max_idx = 0;
 for (int i = 1; i < size; i++) {
 if (arr[i] > arr[max_idx]) max_idx = i;
 }
 return max_idx;
}


/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Supply configuration update enable
 */
 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

 /* MPU Configuration */



void MPU_Config(void)
{
 MPU_Region_InitTypeDef MPU_InitStruct = {0};

 /* Disables the MPU */
 HAL_MPU_Disable();

 /** Initializes and configures the Region and the memory to be protected
 */
 MPU_InitStruct.Enable = MPU_REGION_ENABLE;
 MPU_InitStruct.Number = MPU_REGION_NUMBER0;
 MPU_InitStruct.BaseAddress = 0x24000000;
 MPU_InitStruct.Size = MPU_REGION_SIZE_512KB;
 MPU_InitStruct.SubRegionDisable = 0x87;
 MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
 MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
 MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
 MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
 MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
 MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;

 HAL_MPU_ConfigRegion(&MPU_InitStruct);
 /* Enables the MPU */
 HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);

}

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

This is my main.c file main loop. I call cubeai to generate code file app-cube-ai.c file inside the function. The model initialization was successful, and the model parameters were successfully matched. However, there was a delay in the model inference. The code for Caton is: int result = ai_mnetwork_run(network_handle, &input_buf, &output_buf); . I went inside the model inference function and found that Caton's code was if (inn)
return inn->entry->ai_run(inn->handle, input, output);
else
return 0; Please help me

This topic has been closed for replies.

1 reply

Julian E.
ST Technical Moderator
March 4, 2025

Hello @masirwlw ,

 

I don't really understand your issue is. Can you please try to explain it differently.

In the meantime, here is the documentation if it can be of any help: https://stedgeai-dc.st.com/assets/embedded-docs/embedded_client_api_legacy.html

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.