2019-07-25 1:30 AM
Hi,
I checked UART register of Chorus 4M my environment.
If I would like to set AUTOWU bit in LINCR1 register, is following sequence right?
linflexlp->LINCR1.R = 1; /* enter INIT mode */
linflexlp->LINCR1.R = 0x1001; /* set AUTOWU */
linflexlp->LINCR1.R = 0x1000; /* exit INIT mode */
When I wite '0' (0x00000000) to LINCR1 register to exit INIT mode like serial_lld.c in SPC5Studio (following), not only INIT bit but also other bits on LINCR1 register is clear. Is it right?
/* Leaves the configuration mode.*/
linflexlp->LINCR1.R = 0;
If it is right, I think it is very important behavior.
Best Regards,
Tsutsumi
2019-08-19 11:44 PM
Hi Tsutsumi-sun,
your sequence of instructions is correct. You can also use the following sequence:
SD1.linflexlp->LINCR1.B.INIT = 1; /* enter INIT mode */
SD1.linflexlp->LINCR1.B.AWUM = 1; /* set AUTOWU */
SD1.linflexlp->LINCR1.B.INIT = 0; /* exit INIT mode */
Best Regards,
Luigi
2019-08-19 11:55 PM
Hi Luigi-san,
Thanks you for your sending answer.
I understand.
Best Regards,
Tsutsumi