2022-01-31 2:01 AM
Hi there,
I was looking for the current limit on the 5v and 3.3v pins of the SPC58E80E5 board (I check in the user manual) but I can't figured out.
Which ones are they? Where I can get this information?
2022-01-31 2:49 AM
Hello,
you can find current limits in SPC58 C line datasheet:
Best Regards,
-Olivier
2022-01-31 7:16 AM
I'm not sure if the values below are the ones I was looking for (this is page 34 of the datasheet you pointed to me)
2022-02-02 3:48 AM
Hello,
the two parameters you need to satisfy for reliability and functionality are the ones passed in DS rev8 4.8.3.
"In order to ensure device reliability, the average current of the I/O on a single segment
should remain below the IRMSSEG maximum value.
In order to ensure device functionality, the sum of the dynamic and static current of the I/O
on a single segment should remain below the IDYNSEG maximum value."
Best Regards,
Giuseppe