cancel
Showing results for 
Search instead for 
Did you mean: 

SPC570s-DISP board: FlexCAN sends bad frames independent of CAN parameters

BEdel.1
Associate II

Hello,

I have similar problem with the SP570S-DISP board as described here:

https://community.st.com/s/question/0D50X0000ArRejNSQS/spc570-can-outputs-bad-frame-independent-of-frame-parameters

My Configuration: 250KBaud, 16Tq, Sample-point=75%, XOSC 40MHz, CAN_clk 40 MHz, V_ext=12V/VDD_HV_IO=5V, Vector VN1610+CANoe running, 120 Ohm on both sides, ID=0x135, Data={0xAA, 0x55, 0x00, 0x00, 0xAA, 0x55, 0x00, 0x00} DLC=8.

 Clock settings:

/* Setting the system dividers to their final values.*/
    /*
     * b0     : DE = 0b1  enable divider
     * b9-15  : DIV (Divider is DIV + 1)
     */
    /* System clock 0 divider */
    MC_CGM.SC_DC0.R = 0x80000000UL;
    /* System clock 1 divider */
    MC_CGM.SC_DC1.R = 0x80010000UL;
    /* System clock 2 disabled */
    MC_CGM.SC_DC2.R = 0UL;
 
    /* Pit clock divider 5 */
    MC_CGM.AC0_DC0.R = 0x80040000UL;
    /* SAR ADC clock divider 25 */
    MC_CGM.AC0_DC1.R = 0x80180000UL;
    /* CTU clock divider 25 */
    MC_CGM.AC0_DC2.R = 0x80180000UL;
    /* DSPI clock divider 4 */
    MC_CGM.AC0_DC3.R = 0x80030000UL;
    /* LinFlex clock disabled */
    MC_CGM.AC0_DC4.R = 0UL;
    /* eTimer clock divider 4*/
    MC_CGM.AC0_DC5.R = 0x80030000UL;
    /* FlexCAN clock divider 1 */
    MC_CGM.AC1_DC0.R = 0x80000000UL;
 
    /* Setting the clock selectors for PIT, SAR, CTU, DSPI, LinFlex, eTimer:  PLL_0 */
    /*
     * b4-7: SELCTL     (Auxiliary clock source selection control)
     * */
    MC_CGM.AC0_SC.R = 0x02000000UL;
    /* Setting the clock selectors for FlexCAN: XOSC (external oscillator) */
    MC_CGM.AC1_SC.R = 0x01000000UL;
    /* Setting the clock selectors for PLL_0: XOSC (external oscillator) */
    MC_CGM.AC2_SC.R = 0x01000000UL;
    /* Setting the clock selectors for PLL_1: XOSC (external oscillator) */
    MC_CGM.AC3_SC.R = 0x01000000UL;

FlexCAN settings:

uint8_t mb_index = 0;
 
    /* set peripheral clock mode.*/
    cpu_set_peripheral_clock_mode(79U, 0x12);
 
    /* external clock source */
    FLEXCAN_0.CTRL.B.CLK_SRC = 1U;
 
    /* Empty all mailboxes */
    for (mb_index = 0; mb_index < 8U; mb_index++) {
        FLEXCAN_0.MB[mb_index].MB_CS.R = 0UL;
        FLEXCAN_0.MB[mb_index].MB_ID.R = 0UL;
        FLEXCAN_0.MB[mb_index].MB_DATAL.R = 0UL;
        FLEXCAN_0.MB[mb_index].MB_DATAH.R = 0UL;
    }
 
    /* Enable the device.*/
    FLEXCAN_0.MCR.B.MDIS = 0U;
 
    while (0 == FLEXCAN_0.MCR.B.LPM_ACK)
        ;/* wait until module is enabled */
 
    FLEXCAN_0.MCR.B.FRZ = 0b1;
    FLEXCAN_0.MCR.B.HALT = 0b1;
 
    while (0 == FLEXCAN_0.MCR.B.FRZ_ACK)
        ;/* enter freeze mode */
 
    FLEXCAN_0.MCR.B.MAXMB = 7U;
 
    FLEXCAN_0.MCR.B.SUPV = 0b0; /* deactivate super-visor mode */
    FLEXCAN_0.MCR.B.SRX_DIS = 0b1; /* No self reception*/
    FLEXCAN_0.MCR.B.FEN = 0b0; /* No Fifo */
    FLEXCAN_0.MCR.B.AEN = 0b0; /* No Abort enable */
    FLEXCAN_0.MCR.B.WRN_EN = 0b1;
    FLEXCAN_0.MCR.B.LPRIO_EN = 0b0; /* no prio */
 
    (void) FLEXCAN_0.TIMER.R; /* Unlock message buffer */
 
    /* RX MB initialization.*/
    for (mb_index = 0U; mb_index < 4U; mb_index++) {
        FLEXCAN_0.MB[mb_index].MB_CS.B.CODE = 4U;
    }
 
    /* TX MB initialization.*/
    for (mb_index = 4U; mb_index < 8U; mb_index++) {
        FLEXCAN_0.MB[mb_index].MB_CS.B.CODE = 8U;
    }
 
    FLEXCAN_0.CTRL.B.PSEG1 = 5U;
    FLEXCAN_0.CTRL.B.PSEG2 = 3U;
    FLEXCAN_0.CTRL.B.PROPSEG = 4U;
    FLEXCAN_0.CTRL.B.PRESDIV = 9U;
    FLEXCAN_0.CTRL.B.RJW = 1U;
    FLEXCAN_0.CTRL.B.SMP = 0b0;
 
    FLEXCAN_0.CTRL.B.LBUF = 0b1; /* Lowest buffer first */
    FLEXCAN_0.CTRL.B.TWRN_MSK = 0b1;
    FLEXCAN_0.CTRL.B.RWRN_MSK = 0b1;
    FLEXCAN_0.CTRL.B.BOFF_MSK = 0b1;
    FLEXCAN_0.CTRL.B.ERR_MSK = 0b1;
    FLEXCAN_0.CTRL.B.LOM = 0b0; /* listen-only */
    FLEXCAN_0.CTRL.B.LPB = 0b0; /* loop back */
    FLEXCAN_0.CTRL.B.TSYN = 0b0;
 
    FLEXCAN_0.MCR.B.FRZ = 0U;
 
    while (1 == FLEXCAN_0.MCR.B.FRZ_ACK)
        ;/* leave freeze mode */
 
    /* IRQ setting for TX buffers */
    FLEXCAN_0.IMASK1.R = 0xFFFF0000UL;
 
    /* Clear interrupt flags with ones */
    FLEXCAN_0.IFLAG1.R = 0xFFFFFFFUL;
 
    /* Synchronize to CAN bus */
    FLEXCAN_0.MCR.B.HALT = 0U;

Transmit section:

/* clear IRQ flags with ones */
        FLEXCAN_0.IFLAG1.R = 0xFFFFFFFUL;
 
        /* Lock message buffer */
        (void) FLEXCAN_0.MB[0].MB_CS.B.CODE;
 
        /* clear data fields */
        FLEXCAN_0.MB[buffer].MB_DATAL.R = 0U;
        FLEXCAN_0.MB[buffer].MB_DATAH.R = 0U;
 
        /* inactivate buffer */
        FLEXCAN_0.MB[buffer].MB_CS.B.CODE = 0b1000;
 
        FLEXCAN_0.MB[buffer].MB_ID.R = frame->id << 18U;
 
        /* Fill in data...*/
 
        FLEXCAN_0.MB[buffer].MB_CS.B.LENGTH = frame->dlc;
        FLEXCAN_0.MB[buffer].MB_CS.B.IDE = 0U; /* standard id */
        FLEXCAN_0.MB[buffer].MB_CS.B.RTR = 0U; /* data frame */
        FLEXCAN_0.MB[buffer].MB_CS.B.SRR = 0U;
 
        /* start transmission */
        FLEXCAN_0.MB[buffer].MB_CS.B.CODE = 0b1100;

EDIT:

I am getting directly after transmit with "buffer" set to a TXD buffer this signal on the bus:

0690X00000DBntYQAT.png

0690X00000DBntxQAD.png

0690X00000DBnu7QAD.png

(obviously CANoe is sending error frames)

I discovered when I do a non fitting initialization of message boxes but with a number less than the MAXMB value then I get this signal instantly after FLEXCAN_0.MCR.B.FRZ = 0U during init.

And I have the same problem with the examples delivered with SPCStudio.

With Loop-back activated there are no problems.

Thank you in advance!

Regards

Ben

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
DCARR
Associate III

Hi,

I think that there is a problem in pads configuration.

Please configure the right RX and TX pads as showed in the below example:

   

  /* Setup FlexCAN 0 pins */

  /* TX (PB0)

    PA = 1 (AF1) / OBE = 1 / ODE = 1 / WPE = WPS = SRC (min value) = 0 */

  SIU.PCR[16].R = 0x0620;

  /* RX (PB1)     IBE = 1 */

  SIU.PCR[17].B.IBE = 0x1;   

Best regards

Domenico