cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5_Studio_LoadAddress

baskar
Associate II
Posted on August 03, 2016 at 11:17

SPC5_Studio_LoadAddress

We are in completing stage of the project and our application size is 

122K.

We want to load new application in different sector 5 or 6,so how to generate the code using spc5 studio.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Erwan YVIN
ST Employee
Posted on August 10, 2016 at 10:02

Hello Rosen ,

Do you use RLA or HAL ?

you can change the load address in the platform component

it updates the linker file

Best regards

Erwan

________________

Attachments :

2016-08-10_100138.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qX0g&d=%2Fa%2F0X0000000boc%2F0Pm4gvkGlB3uLqIDrc7aSiOQd4OzDnP5T_fSqr736aM&asPdf=false