cancel
Showing results for 
Search instead for 
Did you mean: 

Origin of ppc-freevle-eabi toolchain?

davedave95
Associate III
Posted on December 07, 2016 at 09:13

Hello,

I would like to make a native Linux build of the ppc-freevle-eabi toolchain that is shipped with SPC5Studio; the toolchain comes with a readme.txt with some release notes, but it does not state the origin or where sources can be found.

Can anyone shed some light on this? Are the sources available as a whole, and if not, are the changes made to the default 4.9.2 gcc available somewhere?

Thank you,

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Erwan YVIN
ST Employee
Posted on December 07, 2016 at 09:57

Hello Gert ,

The gcc

ppc-freevle-eabi toolchain 

(4.9.2) is coming from NXP-Freescale side.

the source code is coming from nxp community.

https://community.nxp.com/docs/DOC-333045

 

We are using the similar core on PowerPC microcontrollers (MPC56-SPC56)

Linux version is working well.

           Best regards

                                      Erwan