2017-01-21 9:58 PM
Hello, I configured in enhanced mode for system clock generation, our input clock is 40Mhz external crystal and need to generate 150Mhz system clock. Since hardware is not supported to check CLKOUT pin for system clock, we configured SCK clock for calculating system clock.
NOTE: For above configuration the parameters values EPREDIV, ERFD and EMFD is not satisfying for 150Mhz system clock generation if we substitute in enhanced mode formula. Im confused!!!!!
Please do needful and give us solution resolve this issue, the project is in critical condition. If any documents related to issue please do share to my ID below mentioned.
Regards
Mahesh chamaraja
Office ID :
mailto:mahesh.chamaraja@kpit.com
Phone No : +917259205624
##clock ##spc56 ##fmpllSolved! Go to Solution.
2017-02-21 2:41 AM
Hello Mahesh ,
sorry the RM is not cleared
You should respect some steps
Step 1
Support for 50MHz system clock generation
The oscillator and PLL support generation of a 150 MHz system clock while using the 40 MHz crystal required for FlexRay operation. A possible PLL configuration is shown below: �?Input clock (crystal frequency): 40 MHz
�? EPREDIV/IDF divider = /8 (1–15 range supported) �? EMFD/NDIV loop divider = 80 (32–96 supported) �? VCO clock out = 300 MHz (256–512 MHz range supported) �? ERFD/ODF output divider = /2 (/2, /4, /8, /16 supported) �? SYSDIV divider = /1 (/1, /2, /4, /8, /16 supported) �? System clock = 50 MHzStep 2
wait for Lock the PLL
Step 3
Support for 50MHz system clock generation
The oscillator and PLL support generation of a 150 MHz system clock while using the 40 MHz crystal required for FlexRay operation. A possible PLL configuration is shown below: �?Input clock (crystal frequency): 40 MHz
�? EPREDIV/IDF divider = /8 (1–15 range supported) �? EMFD/NDIV loop divider = 60 (32–96 supported) �? VCO clock out = 300 MHz (256–512 MHz range supported) �? ERFD/ODF output divider = /2 (/2, /4, /8, /16 supported) �? SYSDIV divider = /1 (/1, /2, /4, /8, /16 supported) �?System clock = 150 MHz
Step 4
wait for Lock the PLL
==> It is ok for my side
/**
 * @brief SPC563 clocks and PLL initialization.
 * @note All the involved constants come from the file @Community memberoard.h and
 * @p hal_lld.h
 * @note This function must be invoked only after the system reset.
 *
 * @special
 */
void spc_clock_init(void) {
#if !SPC5_NO_INIT
 /* PLL activation.*/
 FMPLL.ESYNCR1.B.EMODE = 1; /* Enhanced mode on. */
 FMPLL.ESYNCR1.B.CLKCFG &= 1; /* Bypass mode, PLL off.*/
#if !SPC5_CLK_BYPASS
 FMPLL.ESYNCR1.B.CLKCFG |= 2; /* PLL on. */
 FMPLL.ESYNCR1.B.EPREDIV = SPC5_CLK_PREDIV;
 FMPLL.ESYNCR1.B.EMFD = SPC5_CLK_MFD;
 FMPLL.ESYNCR2.B.ERFD = SPC5_CLK_RFD;
 while (!FMPLL.SYNSR.B.LOCK)
 ;
 FMPLL.ESYNCR1.B.EMFD = 60;
 while (!FMPLL.SYNSR.B.LOCK)
 ;
 FMPLL.ESYNCR1.B.CLKCFG |= 4; /* Clock from the PLL. */
#endif /* !SPC5_CLK_BYPASS */
 /* SYS Clock Divider setting.*/
#if (SPC5_SIU_SYSDIV_BYPASS == TRUE)
 SIU.SYSDIV.B.BYPASS = 1U;
#else
 SIU.SYSDIV.B.BYPASS = 0U;
 SIU.SYSDIV.B.SYSCLKDIV = (uint8_t)SPC5_SIU_SYSDIV_SYSCLKDIV;
#endif
 /* Setting up RAM/Flash wait states and the prefetching bits.*/
 ECSM.MUDCR.R = SPC5_RAM_WS;
 FLASH_A.BIUCR.R = SPC5_FLASH_BIUCR | SPC5_FLASH_WS;
 FLASH_A.BIUCR2.R = 0;
#if !defined(_SPC564A70_)
 /* The second controller is only present in Andorra 3M or 4M.*/
 FLASH_B.BIUCR.R = SPC5_FLASH_BIUCR | SPC5_FLASH_WS;
 FLASH_B.BIUCR2.R = 0;
#endif /* !defined(_SPC564A70_) */
 /* CAN Clock Divider setting.*/
 SIU.SYSDIV.B.CAN_SRC = (uint8_t)SPC5_SIU_SYSDIV_CAN_SRC; 
#endif /* !SPC5_NO_INIT */
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?Best regards
Erwab
2017-03-14 2:34 AM
Hello Erwan,
Sorry for the delay
Can I know the values for this macros?
SPC5_FLASH_WS
SPC5_FLASH_BIUCR