2017-03-10 6:52 AM
Hi, is it possible to lock out debugger access after programming the DCF record in the UTEST memory region?
I am using the
SPC570S40E1 micro and the Lauterbach debugger. After programming a DCF record incorrectly, I am getting a 'debug port fail' error when entering these commands: �SYStem.DETECT CPU� or �SYStem.Up�.
How do I go about unlocking the device?
Thanks
#censored #spc570s40e1 #dcf2017-03-16 3:40 AM
Hello ,
you should configure your debugger to enter the password NVPWD1/NVPWD2
the default password is 0xFEED_FACE_CAFE_BEEF.
Best regards
Erwan
2017-03-16 8:07 AM
Hey Erwan, I have tried the command '
SYStem.option.keycode 0xFEEDFACECAFEBEEF' , but it didn't work.