2020-01-27 7:16 AM
Hi,
I am able to work on ADC0 and ADC1 in separate code ( LED11 flashes properly as per the analog signal). But when I initialise ADC0 and ADC1 in the same code, LED11 AND LED12 flashes as per the analog signal at ADC1.
(I am using ADC sample code with addition of ADC0 , no error program compiled properly)
Please help me to resolve the issue.
Thanks and Regards,
Pradnya
2020-01-28 8:17 AM
2020-01-28 8:51 AM
Hello Ervan,
With SPC560P-DISP BOARD, I initialised ADC0 ( Analog input from Pot R58 available on board) , checked with LED11 flashing and then in same code I initialised ADC1 ( Analog input from Pot R57 available on board) , checked with LED12 flashing.
But when I changed analog input at ADC1 (POT R57), flashing rate of LED11 also get change along with LED12.
Flashing rate of LED11 is not expected to change since it is assigned to ADC0.
Please guide,
Thanks and Regards,
Pradnya