2021-07-26 12:47 AM
Hi i have a custom board with SPC560B50L3 that is in the SPC560BC Family.
There is no SPC560BC xx Firmware Updater Component.
If i try to add it (with shw incompatible components) of course i have problem generation files.
There is some alternative?
Thanks
Solved! Go to Solution.
2021-07-27 11:24 PM
OK, i copy all files and folders and component.mak from SPC560B xx Firmware Updater Component and it works!
2021-07-27 11:24 PM
OK, i copy all files and folders and component.mak from SPC560B xx Firmware Updater Component and it works!
2021-09-17 1:15 AM
Normally ,
if the component is incompatible , generation is failing , it is normal
could you check Firmware Updater test application ?
Best Regards
Erwan