Skip to main content
Basavanagouda1
Associate II
January 3, 2020
Solved

Bootloader example code for SPC560P50L3 controller

  • January 3, 2020
  • 3 replies
  • 1752 views

Hi All,

I'm searching for example Bootloader code for SPC560P50L3 controller ( 100 pins package). I tried import from the example code in SPC5 studio, but it is for a SPC560P50L5 controller.

How I can convert this code SPC560P50L35controller ( 144 pins package). I need to match the controller pin mapping

Is there any way to convert this code to 100 pins package controller OR is there any bootloader example code available for SPC560P50L3 controller, where i can find it.

Please suggest me the link or method to convert it.

Thanks,

Basava.

This topic has been closed for replies.
Best answer by Tesla DeLorean

If you have an understanding of the two controllers, and the differences, you should be able to port code from one to the other.

Perhaps have a conversation with the sales and support engineers assigned to your project, and have them provide a list of contractors familiar with the hardware who could provide assistance on your project.

3 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
January 3, 2020

If you have an understanding of the two controllers, and the differences, you should be able to port code from one to the other.

Perhaps have a conversation with the sales and support engineers assigned to your project, and have them provide a list of contractors familiar with the hardware who could provide assistance on your project.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Basavanagouda1
Associate II
January 6, 2020
Basavanagouda1
Associate II
January 6, 2020

Thank you for the reply,

I figured it out, we can choose MCU package from Platform settings in SPC560 studio