Associate III
April 25, 2015
Question
Application Configuration - Clock settings
- April 25, 2015
- 3 replies
- 1195 views
Posted on April 25, 2015 at 13:58
I am using test application for serial interface with SPC560D30. I used the application configuration - clock settings as 16MHz with the SPC discovery kit. Now keeping the test application same, I want to change the clock settings to 8MHz which the actual value I am using on my target hardware. When I do these changes using Application configuration and generate it, following errors are displayed (please find attached image also),
In file included from ./components/portable_spc5_hal_component/lib/include/hal.h:32:0,from ./components/portable_spc5_hal_component/lib/src/hal_queues.c:38:
./components/spc560dxx_hal_drivers_component/lib/include/hal_lld.h:683:2: error: #error ''SPC5_FMPLL0_VCO_CLK outside acceptable range (SPC5_FMPLLVCO_MIN...SPC5_FMPLLVCO_MAX)''
In file included from ./components/portable_spc5_hal_component/lib/include/hal.h:32:0,
from ./components/portable_spc5_hal_component/lib/src/can.c:25:
./components/spc560dxx_hal_drivers_component/lib/include/hal_lld.h:683:2: error: #error ''SPC5_FMPLL0_VCO_CLK outside acceptable range (SPC5_FMPLLVCO_MIN...SPC5_FMPLLVCO_MAX)''
In file included from ./components/portable_spc5_hal_component/lib/include/hal.h:32:0,
from ./components/portable_spc5_hal_component/lib/src/hal.c:25:
./components/spc560dxx_hal_drivers_component/lib/include/hal_lld.h:683:2: error: #error ''SPC5_FMPLL0_VCO_CLK outside acceptable range (SPC5_FMPLLVCO_MIN...SPC5_FMPLLVCO_MAX)''
In file included from ./components/portable_spc5_hal_component/lib/include/hal.h:32:0,
from ./components/portable_spc5_hal_component/lib/src/adc.c:25:
./components/spc560dxx_hal_drivers_component/lib/include/hal_lld.h:683:2: error: #error ''SPC5_FMPLL0_VCO_CLK outside acceptable range (SPC5_FMPLLVCO_MIN...SPC5_FMPLLVCO_MAX)''
Does that mean clock settings below 16MHz are not allowed? Whether SPC560D30 can not support/use 8MHz xtal?Your earliest response will be highly appreciated as this will affect xtal and other parts procurement and may affect the delivery schedule. Thanks in advance for your help.Mike.