2015-07-11 12:29 AM
Dear Forum members,
In one of my application, I need to drive photo LED of IL300 through TLO64. But it is not working. If I just replace TLO64 with TLO74, everything works proper. My initial guess was that TLO64 might not be supplying sufficient current. But looking at datasheet, I didn't find any major deviation in output current graph of both these IC's. Am I missing something?2015-07-13 01:41 AM
Hello,
The TL074 and TL064 op-amps do not have exactly the same output capabilities. Actually, the TL074 is able to drive more current. In the figure below, you can find a comparison between typical parts of TL064 and TL074. In addition, thanks to its higher supply current, the TL074 has a bigger GBP, bigger SR and a lower noise. - GBP : 4MHz (1MHz for the TL064) - SR : 16V/µs (3.5V/µs for the TL064)