cancel
Showing results for 
Search instead for 
Did you mean: 

The question for the Class-D audio amplifier IC "TDA7498"

michifuji
Associate

Is the internal circuit of the terminal damaged if a surge voltage of 3.6V or higher is applied to the INP and INN terminals of the Class-D audio amplifier IC "TDA7498"?

Is there an element in the chip to protect against the effects of surge voltage?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0