cancel
Showing results for 
Search instead for 
Did you mean: 

I'm searching for a VNLD5090-E substitute, can someone help me out?

PLeon.2
Associate
 
3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @PLeon.2​, to the community!

For the VNLD5090, only the tube packaging unit is discontinued and no longer available, but Tape&Reel can still be ordered.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello Peter,

I tried to find this component on all the internet with no luck, the only one I found available comes from alibaba at almost 4 times the price.

Regards

Since the beginning of the pandemic, we have unfortunately been experiencing completely abnormal times, which is also reflected in the availability of components. However, the community is the wrong place to look for components, because the community can be seen as a reference work and technical or comprehension questions are discussed.

In this respect, I would ask you to contact your local dealer, even if some components are currently difficult to very difficult to find.

However, I would like to take this opportunity to point out that there are a disturbingly large number of fakes on offer, especially from non-official dealers, which are even marked to look very genuine, because the high achievable price attracts counterfeiters.

Nevertheless, I hope to have helped a little.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.