2023-04-11 01:15 AM
Hi, I'm trying to design hifi amplifier using TDA7292 refering its datasheet.
I read the datasheet of TDA7292, and I have some following questions :
I'm newbie in circuit design, so please understand me if there are any sound like dumb question.
Thank you! 😀
2023-04-11 01:16 AM
Here's the datasheet of TDA7292 :
2024-01-17 11:18 PM
Hi,
In datasheet there is no Bridge Circuit and recommended supply details. If I want to convert single output capable to drive 80W max.
Can Any one provide the Bridge Circuit Schematic and recommended supply for bridge circuit.
2024-01-18 12:47 AM - edited 2024-01-18 12:49 AM
Hi,
try:
2024-01-18 06:02 AM
How can I use differential audio input at TDA7292? Is it okay to connect amplifier's IN1- and IN2- pin to differential audio source's L- and R- pin instead of connecting those amp pins to GND?
L & R is not differential outputs, but single ended left & right.
With a single supply circuit, is it okay to supply single +48V 2A power to TDA7292? In TDA7292's electrical absolute maximum ratings, it the maximum DC supply voltage of TDA7292 is +-35V. But what I'm trying to design is single supply circuit. I wonder if it would be overloaded.
You can use single power, +70V
Is there are any disadvantage using 'For Single supply' circuit instead of using 'For Dual rail supply' circuit?
Yes, there is disadvantage in using electrolitic capacitors, find a DS for TDA2030 and study amp with single power.
I found what I assume to be an error in the Figure22 diagram on page 17 in the datasheet. Pin 2 of the TDA7292 is OUT1 and pin 10 is IN1-, but in Figure 22 they are reversed. It seems to me that this is an error, am I right?
Agree, typo error. Use pin desciption with figure 2