Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Hi,I have a NUCLEO-WL55JC (revision 0E) that stop working after I flashed the LoRaWAN_End_Node example project. With the CubeProgrammer, sometimes I can manage to update the STLink Firmware (if I keep rebooting the board), but I can't ever connect to the main MCU.I was wondering if there is any jumper configuration that allows flashing the main MCU from an external STLink (I'm not sure If it will fix the issue, but let's try it).Thank you!
We are working on "Peripheral Lite" from STM32WB_FW and we would like to include SPI and UART libraries . We imported this project in STM32 IDE by automatic conversion. Since there is no "ioc" file (CUBEMX) and only a small part of HAL libraries are present, how can we add the other part?
Hi, We are trying to configure device keys using AT commands. We are able to change the App EUI and Device EUI using AT commands. But we are facing issues when modifying the App key and NWK key using AT commands. We referred the AT commands configuration examples of STM32WLE5 . But there is no reference for configuring App key and NWK key. Is it possible to change App key and NWK key using AT commands ? Please guide us with any references or ideas :).RAK Module Details:https://docs.rakwireless.com/Product-Categories/WisDuo/RAK3172-Module/Overview/#product-descriptionThanks!
I am aware there is a datasheet, but it does not contain the info I need. I am trying to configure timer triggered timers for my project, so I would like to know the internal trigger mapping for each timer. I am hoping to find something similar to the image below from the STM32F446xx reference manual. Any help is appreciated.
Hi, I'm using the STM32WB55 as a BLE peripheral. The goal is to support multiple simultaneous connections with different Centrals, so that the peripheral can broadcast its characteristics to multiple clients.To accomplish that, my code re-enables advertising after a connection has been established, e.g. in EV_LE_CONN_COMPLETE I call aci_gap_set_discoverable() again. This works exactly two times (using the custom template generated by CubeMX). However, after the second central connects, additional aci_gap_set_discoverable() calls fail with the error 0x0C. Any pointers on why this is happening is greatly appreciated.
Reference manual RM0453 and AN5457 - Rev 2 give some info on optimal PA and TxParm settings but the data is incomplete and appears to be inconstant. For example, Table 2 of AN5457 says for RFO_HP, +14dBm set paDutyCycle to 0x2 and TxParms to 14. The ref manual Table 35 says for RFO_HP, +14dBmset PaDutyCycle to 0x02 and Txparms to 0x16 (dec 22)So do I set Txparms to 14 or 22?paDutyCycle for +15dBm RFO_LP are also inconsistent. The ref manual says 0x7 and the ap-note says 0x06.Further the tables are incomplete. For example, under HP only settings for output powers of 22,20,17,14 are provided. I tried to interpolate between values but had issues there. And guidance for power lower the 10 (LP) and 14 (HP) dBm are missing.Is there a document or guidance with more complete information? Which tables should I believe? The Reference manual or the Ap-Note? What settings should I use (for example) for LP at 5dBm or other powers below 10/14 dBm. Maybe for powers below a certain value just set paCo
Hi, I have a Nucleo WB55 board and I am testing some example projects.I noticed I cannot see any data from com port for MAC_802_15.4 example, however when I have flash the Phy_802_15_4_Cli example, it works. Do I need to enable some extra settings for the mentioned project to see data from serial?Thanks.
Hi,I have a problem on the LoRa transmission.If I use STM32F103 on SPI 1, LoRa transmission works.And if I use the STM32G070 with the same code the LoRa transmission doesn't work.What is the différence on the SPI in the STM32G070 ?
Given interrupt continuously when lora joining process occurred, at that time the device is restarted.why?
I'm trying to logging Teseo LIV3FL using my STM32 Nucleo-WL55JC1. I've tried in my ESP32 before and it works as it is. However, when I tried to use them in my Nucleo board, the message are messy or mixed between other messages. Expected Output:Received Data: $GPGGA,081020.000,0745.76016,S,11023.30496,E,0,03,99.0,186.70,M,0.0,M,,*79Current Output:$GPGGA,081020.000,0745.Received Data: 76016,S,11023.30496,E,0,03,99.0,186.70,M,0.0,M,,*79I suspect it caused because the UART is still busy when I send another message. Any workaround how to manage the messages so they didn't mixed up?
Is there a simple example for STM32WL55 that does not use the sequencer?I want to integrate the LoRa radio with my code and my own task scheduler.From CubeMX, the SUBGHZ module works well but when I add SUBGHZPhy, everything seems to break.
Hello community,We are using STM32WL V1.2.0 to develop an application based on the example application "LoRaWAN_End_Node_FreeRTOS". Board: Nucleo-WL55JC1. The example application works.However, as soon as we add the function "osDelay(2000)" in a thread, the application gets stuck in tasks.c, line 2581:configASSERT( ( xTickCount + xTicksToJump ) <= xNextTaskUnblockTime );Steps to reproduce: LoRaWAN_End_Node_FreeRTOS, lora_app.c, line 439: add code: APP_LOG(TS_ON, VLEVEL_M, "before osDelay(2000)\r\n"); osDelay(2000); APP_LOG(TS_ON, VLEVEL_M, "after osDelay(2000)\r\n");We suspect that the ticks are not updated correctly, so that after waking up from sleep, configASSERT() is hit because the system thinks it has missed xNextTaskUnblockTime.When using FreeRTOS timers osTimerNew(), osTimerStart(), the same happens. The original example application uses neither osDelay() nor osTimerNew(), but only osThreadFlagsWait/Set() functions, and therefore works fine.FreeRTOS configuration: as in th
I am using the STM32WLE5, and periodically entering and exiting STOP2 mode. The VBAT is connected directly to VCC. I set PWR_CR1_DBP on system initialization, and assume it should not change. On exiting stop mode, sometimes the DBP bit is randomly cleared - causing subsequent writes to the RTC to fail.My code below is my stop mode entry routine, and I observe the DBP bit being cleared directly after stop mode. Note I have disable IRQ's to eliminate the possibly of this being cleared during an ISR.void CORE_Stop(void) { CRITICAL_SECTION_BEGIN(); HAL_SuspendTick(); MODIFY_REG(PWR->CR1, PWR_CR1_LPMS, PWR_LOWPOWERMODE_STOP2); SET_BIT(SCB->SCR, SCB_SCR_SLEEPDEEP_Msk); if (!(PWR->CR1 & PWR_CR1_DBP)) { // This never occurrs __BKPT(); } __WFI(); if (!(PWR->CR1 & PWR_CR1_DBP)) { // This seems to occurr randomly __BKPT(); } CLEAR_BIT(SCB->SCR, SCB_SCR_SLEEPDEEP_Msk); CLK_InitSYSCLK(); // Equivilent to SystemClockConfig HAL_Resu
Hello to everyone. I have the STM32WLE board and I have an external Sx1276 module. STM32WLE board has Sx1262 lora. I am trying to communicate Sx1262 to Sx1276. Actually, when I set Sx1262 as "Transmitter" and Sx1276 as "Receiver", I don't encounter any problems at first. Devices can send and receive data. However, when I set Sx1262 as "Receiver" and Sx1276 as "Transmitter", communication does not occur. The Sx1262 also never falls into the RxDone interrupt. It keeps crashing into RxError interrupt. Please help me!!
I'm planning to make a GPS tracker using Teseo LIV3FL as a slave device and STM32 Nucle-WL55JC1 MCU with I2C communication protocol. The I2C reading is working (I assumed it works since I'm receiveing some data), but the problem is when I take one of the reading and decode it using a GPGGA (or similar) decoder it says I got an invalid data.Serial monitorDecoded dataAnd code snippet for sensor readingwhile (1) { /* USER CODE BEGIN 3 */ if (HAL_I2C_IsDeviceReady(&hi2c1, 0x3A <<1 + 0, 2, 10) == HAL_OK) { HAL_I2C_Master_Receive(&hi2c1, 0x3A <<1 + 0, (uint8_t *)receivedData, sizeof(receivedData), 1000); HAL_UART_Transmit(&huart2, (uint8_t*)receivedData, sizeof(receivedData), 1000); while (HAL_I2C_GetState(&hi2c1) != HAL_I2C_STATE_READY); } else { uint8_t state[10] = "DEVICE IS NOT READY\n"; HAL_UART_Transmit(&huart2, (uint8_t*)state, sizeof(state), 1000); } HAL_Delay(500); }Any idea where did I go wrong? Thank you.
What does the TSC_IOASCR register do?Checked the reference manuals for STM32 WB35xx/WB55xx (RM0434) and F0xx (RM0091) and only get the following information: What's the behaviour of this setting for pins in the various modes (unused, sampling, channel)? I see that it says "Note: These bits control the I/O analog switch whatever the I/O control mode is (even if controlled by standard GPIO registers)." but what does controlling the analog switch mean and how does it relate to TSC?
I wanted to manage routers which are connected to same network. Does Coordinator can manage them or coordinator has any list about connected routers? If there is a list of connected devices please let me know.
..
Hi, i'm trying to update stack via internal firmware. Our device based on STM32WB55: Device ID : 0x495 Revision ID : Rev Y Device name : STM32WB5x Flash size : 1 MBytes Device type : MCU Device CPU : Cortex-M4 BL Version : 0xd5Stack binary file located in internal flash at address 0x080CB000.Below is the data from the programmer: When I call SHCI_C2_FUS_FwUpgrade, the next call to SHCI_C2_FUS_GetState returns the following result - FUS_STATE_ERROR_IMG_NOT_AUTHENTIC.How to solve this problem? Thanx.
We need dedicated drivers for Flash memory Read and Write operations dedicatedly. In example project given the just Read a 32-bit word data only. If we want to read the entire page or part of the page data and verification is there any driver layer available, please share to us.
Hi team,I used STM32WB15CCU6 in my project for Voltage and sensing. I already used all analog pin for sensing.I need one SPI and one UART communications channels.Can you please suggest which pins can I used for SPI and UART.I request please share the schematic or pin mapping details.Thanks & RegardsRajkumar ChaurasiyaMob. No. 8591217827
Hello!There is a board with 2 MCUs, one of them is STM32WB55, second is STM32L4Q5. I need to launch both in boot mode and load firmware over UART. When L4Q5 is in boot mode and UART1 is configured (as mentioned in AN2606) I upload firmware in this MCU and everything is going well. I repeat the same steps with WB55. After I send start frame to WB ( START_FRAME[2] = {0x7F, 0x80};) I get ACK (0x79), but whatever I send next - there aren't ACK, only NACKs (0x1F).What I'm doing wrong? Best regards, Den
Hi,I am working with a STM32WB55RG and by checking the different BLE Stack_full versions available, I realized that their start addresses could vary quite a lot.Is there a guideline for the maximum size that any future BLE stack could have? Example:Right now I am using the BLE stack full 1.13.0 that starts at 0x080C7000. I put the upper limit for my app size at 0x080C5000. How can I know that no further BLE stack versions will be bigger and overlap my application?Best regards.
Hi Team,We are using the STM32WB55 Series for our product. At each power cycle or reset, we need to know what the reason is (like WD Reset, Soft Reset, or Pin Reset, POR reset).Could you please tell me by reading the which register, we came to know the Reset Reason.Regards,Srinivas.V
Hello everyone,We're trying to achieve a low power consumption on a custom board which have a MCU from the STM32WB55 range. I think that I was able to get into stop2 mode as PC was way lower than in sleep mode, and the device could not be detected anymore by the debugger. I reset C2BOOT bit early in main loop and I'm hoping that this Core is effectively halted, even though I don't know how to monitor it on this particular setup. The problem is that PC is still as high as 900µA, which is A LOT compared to what I've seen most of the time on the forums for others MCUs (2µA). Does anyone know what should be the normal PC if the MCU was not on a custom board (i.e. what is the "real" PC of the STM32WB55 in stop2 mode with no peripherals enabled) in order to know if the problem may be on the board that draws a lot of current ? And how can I be sure that Core2 is halted ? Stop2 mode shouldn't be achievable with C2 running (another state than CSTOP, if I understand correctly), and I think that
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.