Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
We are working with android and there are multiple problems it is causing us with its Service Changed characteristic.Is there a way it will not be created? Some chcekbox in CubeMx or else?Cheers!
Hi,We are designing ou custom Lora application based on the STM32WLE5CCU6 MCU.1- We would like to know if there is an eval board that can be used in manufacturing tests to perform a pingpong communication test (between our custom board and the eval board). Is there an AN that decribes such test ?What we ve found is this document that can be used to perform a ping pong test.https://www.st.com/resource/en/application_note/an5406-how-to-build-a-lora-application-with-stm32cubewl-stmicroelectronics.pdfAre there any other related documents ?For the eval board we ve found two boards:https://www.st.com/en/evaluation-tools/nucleo-wl55jc.htmlhttps://www.st.com/en/evaluation-tools/stdes-wl5u2sbb.htmlThe later one do not have any mention to the STM32WLE5CCU6 MCU (Only STM32WL5)Which eval board should be used ?2- Is it possible to generate a continuous waveform from the STM32WLE5CCU6 MCU in order to make frequency and power measurements ?ThanksBR
Hello,Not a question but since I searched for this information and could not locate it anywhere, I post it here to maybe help others.When calling aci_gatt_init(void), it is said that the Service Changed Characteristic is added automatically. /** * @brief ACI_GATT_INIT * Initialize the GATT layer for server and client roles. It adds also the GATT * service with Service Changed Characteristic. [...]The "Service Changed" characteristic is thus always added with the very same handle (which is a requirement for it to be usable), but after that it is basically never mentioned again anywhere in the code or documentation. No info on what this handle is, nor what the payload should be to use it.So here is how to use it from the Server side (to say that things changed), for those like me who want to experiment with variable lists of services in their BLE devices.#define GENERIC_ATTRIBUTE_SERVICE_HANDLE (0x0001) #define SERVICE_CHANGED_CHARACTERISTIC_HANDLE (0x0002) tBleStatus ble_indic
Hi I am using Nucleo-WL55JC1 boards with STMCubeWL firmware version 1.2.0. I have problem with multicast group FUOTA on Lorawan that send package to only one device even though there are more devices in the group. All devices work in class C.Thank you for your help Patryk
I have designed a custom developer board based on STM32WB55CGU6. I have both JTAG and SWD pins on the board. None of them works when I try to connect the board to the STLINK v3MINIE. Except any hardware issues, what else do you suggest for the very first-time flash for a new MCU.
I have successfully implemented a ZigBee coordinator/router with an on/off-server-cluster based on a STM32WB5MMG module.My application is able to form a network and automatically allows certain off-the-shelf ZigBee On/Off-Clients to join the network and bind to the cluster within my device. Persistency is working well, too.As long as my coordinator is fabric new it starts forming the network and allows other devices to join for a certain periode of time.But when there is valid persistence data no additional devices can join, because the network forming process is skipped (I followed the "Zigbee_OnOff_Coord_NVM" example from STM32Cube_FW_WB_V1.16.0).This raises two questions:1) How can I allow more devices to join the network? Wich API functions must I call for that?2) How can I detected that the joining-window has closed on my coordinator?Thank you very much for any hints or help Thomas
I am using a "Sigfox AT Slave" example project. When I type the AT command to get the Sigfox ID or PAC I get an "OK" message as if the command worked, but the ID or PAC do not appear.
My application uses an sx1262 LoRa sub GHz transceiver. I need an MCU which has very low power consumption as well as high performance efficiency. In that case which option will be the best? Is it to choose a lower power series MCU and add an extra transceiver or use STM32WLE5x MCU which has an inbuilt transceiver?
..
Hello,I have a STM32WLE that works with the lora end_node projectI have a sensor that i power up with a mosfet when needed.But during the time that the chip is sleeping i need to disable the internal I2C pullup (+30 uA more due to the fact that the VCC of the sensor don't control the internal pullup).But when i call all the function that can possibly disable the PULLUP (via i2c functions or GPIO_DeInit) the sensor isn't responding even if i call MX_i2c_init()Can someone help meThanks
Hi, I am using the NUCLEO-STM32WL55JC1 LoRaWAN board, which I have connected to the TTN through the OTAA activation method as seen in the snapshot below. Now I wanna connect it via the ABP activation method, however, the device can't connect to the TTN. Can someone let me know what mistake is occurring?
Hi.I am using STM32WL55.I set USART1 with DMA tx and DMA rx.I tried to transmit some data as follows. printf("[*] Program Ver 0.2.0.0\r\n"); printf("\r\n"); printf("Net> ");"[*] Program Ver 0.2.0.0\r\n" and "\r\n" are transmitted.but "Net> " is displayed on terminal.If you change "Net> " to "Net> \r\n" and send it, it will be transmitted normally.What's the problem. How can I fix it.Please, let me know how to resolve the problem.Thank you.
I am developing an application on the Seeed Lora-E5 module, which contains an STM32WLE5.Currently I am programming the device via the SWD interface, but for future firmware updates I want to use the UART, (this UART is available externally through a USB-UART chip).The problem now is how to make the device switch to the internal bootloader : unfortunately the Boot0 (PH3) PIN on the STM32WLE5 is NOT made available on the package of the Seeed Lora-E5 module, so I cannot use that pin..From the AN3155 I see that the CubeMx Programmer is sending 0x7F to the UART, in order for the MCU to select the UART as programming interface. So here is my idea : after reset, I could listen to the UART for eg. 30 seconds, and if in this time a 0x7F byte arrives, jump to the bootloader. (if the 30 seconds expire, the device starts in normal operation mode).I am aware that the bootloader expects the MCU in the same state as after reset, so I will take that into account, be resetting already configured UART (
HelloI'm developing a project on chip STM32WB55. I have referenced the demo aboutBLE-HID of ST's "STM32Cube_FW_WB_V1.16.0". The sample code looks define for mouse usage. Could anyone can teach me how to integrated send volume up key into this sample code (BLE_HID) ?
Hello and good day to you all. I just realised that there were not many articles about the STM32WLE5J in the past and now some topis are added - luckily. And I´m a total beginner to the stm32 enviroment and I really miss a tutorial on how to setup the STM32WLE5J right from the beginning. I can make it to appear in the STM cube MX, but after initializing it via the chip number (it´s a Seed wio e5 mini) the trouble starts. Because there is no board config available and I have to configure everything by myself and thats quite frustrating.Unfortunately most of the tutorials deal with the nucleo board where you get a pre-configured layout out of the box. So maybe someone can make a short video of how to setup a STM32WLE5J all components to start programming? Ideally a Seeed wio e5 mini :)Any tutoria or link will help of course, this would be really great :)Regards Dom
Hello All, Recently I started working on the GNSS with STM32, I am very new to STM32 eco-system. I have a IRNSS click from MikroE which has L89H and I am trying to integrate L89H with STM32WL55JC1 controller. I have implemented the UART with DMA to receive NMEA messages from the L89. I have connected TX, RX, 3,3v, GND pins to STM32's RX, TX, 3.3v, and ground. But when I execute the code no NMEA messages are displayed on the serial monitor. I don't know where I am going wring and I would appreciate to have help for me in this situation. Please let me know if all the connections are correctly done or do I need to connect any additional pins to my STm32 controller. And if any additional information is required to debug the situation I am happy to share the details.Kind regards, Pavan
Hello,I am trying to commissioning NUCLEO-WB55RG Matter thread end device. It fails to commission and connect.Reference Source Code used:Matter beta version for STM32 Github repo: github.com/stm32-hotspot/stm32wb-matter-device-over-thread Setup:1. Matter Thread End DeviceBelow binaries flashed on the STM32 Matter Thread End Device(NUCLEO-WB55).1.1. FUS: "stm32wb-matter-device-over-thread-main\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_FUS_fw.bin" 1.2. BLE Stack: "stm32wb-matter-device-over-thread-main\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_BLE_Thread_ForMatter_fw.bin" 1.3. Application: "stm32wb-matter-device-over-thread-main\Projects\P-NUCLEO-WB55.Nucleo\Applications\Matter\Lighting-App\Lighting-App.bin"2. Border router Raspberrypi(Host) RCP Device(Silabs RCP device)3. Host as a mobile app(chiptool)Also find the Attached logs captured on End device and Android Application while doing commissioning.Please share us th
After some activity using BLE in the background and UART as well as some EXTI on application side, the consumption jumps from 2,4µA to 4mA, so obviously I have a wakelock. If I hotplug to the system afterwards, I can see in PWR_EXTSCR that Stop mode is no longer actually reached (C1STOPF is not set). But checking ISPR I can not see any pending ISRS (the one after Stop is the LPTIM of my OS).What else can prevent the CPU from entering stop? Which registers should I check?
I'm using a STM32WB5MMG chip and I'm trying to receive data with the HAL_UART_Receive_IT() function. But for some reason the HAL_UART_RxCpltCallback function never gets called. Receiving data with blocking mode works, but with an interrupt it doesn't want to workI have enabled the global interrrupt of the USART with CubeMX and I still see that the box is checked.The code I have written should wait until it receives 4 bytes, then echo those bytes back and start waiting again.void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { HAL_UART_Transmit(&huart1, rxBuffer, 4, 100); HAL_UART_Receive_IT(&huart1, rxBuffer, 4); } int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the s
Hello all.I am trying to build up a LoRaWAN end node on a single core STM32WLE5. I am new to LoRa development and thought I would leverage the repo LoRaWAN_End_Node which uses the dual core (STM32WL55 Nucleo). I went ahead in the ioc and tried my best to match up everything HOWEVER there is one piece that seems to be critically different and I don't know how I should set up my settings to account for this....The RTC section on the WL55 seems to be scaled down quite a bit in the Parameter Settings section compared to WLE5......Can someone tell me how to go about setting up the WLE5 RTC section such that it would work for LoRaWAN and be comparable to the WL55 setup? thank you.
Hello,we are currently evaluating whether the STM32WB10 is suitable for a new project. Even though the project will not use wireless connectivity, the STM32WB10 is interesting to us because it is used in high volume in another project and is therefore reasonably priced. According to the data sheet, it comes with 48KB RAM and 320KB flash.Since we will not be using CPU2, SRAM2 will not be used by it. SRAM1 alone is not enough for our application, so we need to have access to at least SRAM2a (36KB) to get our application running.After studying the documentation it seemed to be possible to make SRAM2a and SRAM2b available to CPU1 via the option bytes (RM0478 chapter 3.10.18 and 3.10.19).After trying this out with Nucleo-WB15CC it shows this is not the case at all. I tried configuring FSD, BRSD_A, SBRSA_A, BRSD_B and SBRSA_B, but this did not yield any success.When writing with STM32CubeProgrammer, errors like the following showed up in the log:"Error: Expected value for Option Byte "BRSD_B
STM32 - STM32WB55CGU6 Antenna - 2450AT18B100E Filter - MLPF-WB-01E3 Hello everyone, please help me fix the problem with my custom PCB board and BLE. The antenna on the board won’t work (I don't see my device via Bluetooth) in any way and I don’t know where to look, can anyone implement Bluetooth via filter MLPF-WB-01E3 and antenna 2450AT18B100E on STM32WB? I suspect that there is a problem with the board since I run similar code on Nucleo and I can see the device through my phone but I can't see the device through my phone Does anyone know how to check where the error is, and to check if I designed the board correctly?
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.