Skip to main content
Kimmel1
Visitor II
May 12, 2023 4:00 PM UTC
Question

how can we generate a continuous waveform to measure the output power on a custom board using STM32WLE5CCU6.

Hi,

We are designing ou custom Lora application based on the STM32WLE5CCU6 MCU.

1- We would like to know if there is an eval board that can be used in manufacturing tests to perform a pingpong communication test (between our custom board and the eval board). Is there an AN that decribes such test ?

What we ve found is this document that can be used to perform a ping pong test.

https://www.st.com/resource/en/application_note/an5406-how-to-build-a-lora-application-with-stm32cubewl-stmicroelectronics.pdf

Are there any other related documents ?

For the eval board we ve found two boards:

The later one do not have any mention to the STM32WLE5CCU6 MCU (Only STM32WL5)

Which eval board should be used ?

2- Is it possible to generate a continuous waveform from the STM32WLE5CCU6 MCU in order to make frequency and power measurements ?

Thanks

BR

This topic has been closed for replies.

1 reply

IIRHO.1
ST Employee
Jun 12, 2023 1:47 PM UTC

hello @Kimmel1​ and welcome to st community .

For your first question, you should use the stm32wl55jc card to perform your tests . For the ping pong application and point to point application , i suggest you take a look on this ping pong , P2P application and this video .

For your second question, you can use the MCO (microcontroller clock output) that allows you to output the clock for external MCO pin ( you can also use LSCO for the LSI and LSE clocks) . for more details, take a look to the ref man. And for the power measurements take a look on this training.

If this answers your question, please mount this answer as Best Answer to be defused.

Thanks.

Issam

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.