Skip to main content
AWebe.1
Visitor II
May 20, 2021
Question

SWV not working with STM32F469I-DISCO

  • May 20, 2021
  • 2 replies
  • 3001 views

I'm using a 32F469IDISCOVERY board (Cortex-M4). The integrated ST-Link V2-1 has firmware V2J37M27 and is configured as "Debug + Mass storage + VCP Modus" (default). It doesn't look like it has a jumper or solder bridge to connect SWO and I think it's permanently connected to ST-Link.

I create an new empty project in STM32CubeIDE v1.6.1

  • File -> New -> STM32 Project
  • Board Selector -> STM32F469I-DISCO -> Next
  •  Project Name: swv_foo1, Language: C, Binary Type: Executable, Project Type STM32Cube -> Next
  •  Firmware Package STM32Cube FW_F4 V1.26.1 -> Finish
  •  Initialize all peripherals with their default Mode? -> No
  •  Clock Tree shows SYSCLK is HSI -> 16MHz
  •  change PB3 to SYS_JTDO-SWO
  •  change SYS Debug: "Trace Asynchronous Sw"
  •  Save .ioc -> Generate Code -> YES
  •  Add busy loop to main.c
void Delay (__IO uint32_t nCount)
 {
 while (nCount--)
 {
 }
 }

 and call it in the endless loop, toggle orange LED:

while (1)
 {
 /* USER CODE END WHILE */
 HAL_GPIO_TogglePin (LED2_GPIO_Port, LED2_Pin);
 ITM_SendChar ('x');
 Delay (1000000L);
 /* USER CODE BEGIN 3 */
 }
  •  Project -> Build Project (finished without errors or warning)
  •  Run -> Debug Configurations -> STM32 Corex-M C/C++ Application -> New launch configuration
  •  Debugger -> ST-LINK (ST-LINK GDB server)
  •  Serial Wire Viewer (SWV)
[x] Enable
 Core Clock 16MHz
 SWO Clock: 2000 kHz
 Port number: 61235
 [x] Wait for sync packet
  •  Apply -> Debug
  •   Download and Verifying, Debugger stopps in main at HAL_Init ()

 Tab "SWV ITM Data Console"

   Configure Trace:

     Timestamps

       [x] Enable Prescaler 1

     ITM Stimulus Ports

       [x] 0

     -> Ok

   Port 0 shows up

   -> red filled "record" circle (Start Trace)

 F8 (Resume)

 Orange LED (LED2) starts to blink but

 SWV Trace Log, SWV ITM Data Console, SWV Statistical Profiling keeps empty.

 I've checked DGBMCU_CR and it's 0xe0042004 so

 TRACE_IOEN = 1

 TRACE_MODE = 00: TRACE pin assignment for Asynchronous Mode

 chapter 37.14.2 of the STM32F469xx reference manual says

 0xC5ACCE55 has to be written @E0000FB0 but I'm unsure if this shouldn't be done from the debugger.

 dm00354244-stm32-microcontroller-debug-toolbox-stmicroelectronics.pdf

 doesn't even mention it but I also tried

   volatile uint32_t *ITM_LAR = (volatile uint32_t *)0xE0000FB0; // ITM->LAR

   *ITM_LAR = 0xC5ACCE55; // Enable Access

 but this doesn't change anything.

 I'm really running out of ideas here. Can someone help me?

Thank you, Andy

This topic has been closed for replies.

2 replies

dungeonlords789
Associate III
November 6, 2021

This is ITM example with printf float via ITM.

Also "Output gets flushed on reaching newline character or calling fflush(stdout) function. Additionally there is an option to disable buffering entirely by calling setbuf(stdout, NULL)."

main source: AN4989

see also

1) https://youtu.be/sPzQ5CniWtw

2) https://habr.com/ru/post/440024/

3) http://www.embedded-communication.com/en/misc/printf-with-st-link/

4) https://www.youtube.com/watch?v=Efgp34LbkLU

5) https://mcuoneclipse.com/2016/10/17/tutorial-using-single-wire-output-swo-with-arm-cortex-m-and-eclipse/

0693W00000GWfFFQA1.png0693W00000GWfFKQA1.png0693W00000GWfFAQA1.png0693W00000GWfG3QAL.png

Explorer II
October 6, 2023

The SWO isn't configured or soldered by default, make sure in cubeMX that the SWO is configured (which it looks like you have done). Then close the solder bridge SB7 and the SWV should work. 
I had the same issue and this fixed it for me. 

Sam_Hill333_0-1696577525468.png