cancel
Showing results for 
Search instead for 
Did you mean: 

After flashing done and removing jtag, our application is not working

GAGGA.1
Associate II

I am using STM32F439NIHx MCU. After flashing the code, I removed ST-Link V2 from my PCand restart the MCU but our application is not working. But if I connect ST-Link V2 to my pc then my application is working. What is this problem? Please suggest any solution.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Make sure BOOT0 is pulled low.

Find a UART to use for debug output.

Instrument HardFault_Handler and Error_Handler so it doesn't die silently.

Identify any other infinite while loops that you have, and instrument those or make sure the end up in the Error_Handler and identify the file/line of failure.

Lacking a USART, find a GPIO or LED you can use to signal reaching certain checkpoints or failures.

Enable USART/GPIO in Reset_Handler if failures occurs early in the boot process.

Check supplies and VCAP voltage/capacitors.

Check NRST line.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
GAGGA.1
Associate II

Thanks for your answer.

We have to remove emulator form JTAG port then it is working absolutely working fine.