Associate III
July 23, 2019
Solved
CDC function added but no any com port shown
- July 23, 2019
- 6 replies
- 9483 views
I want to add CDC function. I use the STM32F103RB NUCLEO to add this function. But when I running my application, and insert USB to PC, no COM port shown in PC. I generate the code from cube and I don't know where is the problem. I test WIN10 and WIN7 PC, both are no any port. I have install the related driver in win7