cancel
Showing results for 
Search instead for 
Did you mean: 

PingPong example from I-CUBE-LRWAN software not working on B-L072Z-LRWAN1

pbdiazam
Associate II

As I said in the title, I tried to test the PingPong example avaliable in the I-CUBE-LRWAN software expansion but it does not work on B-L072Z-LRWAN1 board.

After importing the project to SW4STM32 and running it (without doing any modifications), this is what I get in console:

Open On-Chip Debugger 0.10.0-dev-00010-g96aab7b (2018-07-13-06:51)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

srst_only separate srst_nogate srst_open_drain connect_assert_srst

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

adapter speed: 240 kHz

adapter_nsrst_delay: 100

Info : clock speed 1800 kHz

Info : STLINK v2 JTAG v31 API v2 VID 0x0483 PID 0x374B

Info : Target voltage: 3.263434

Info : STM32L072CZYx.cpu: hardware has 4 breakpoints, 2 watchpoints

adapter speed: 240 kHz

target halted due to debug-request, current mode: Thread 

xPSR: 0xf1000000 pc: 0x08002da8 msp: 0x20005000

STM32L0: Enabling HSI16

adapter speed: 4000 kHz

** Programming Started **

auto erase enabled

Info : Device: STM32L0xx (Cat.5)

Info : STM32L flash has dual banks. Bank (0) size is 96kb, base address is 0x8000000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000000e msp: 0x20005000

wrote 36864 bytes from file Debug/mlm32l07x01.elf in 5.673004s (6.346 KiB/s)

** Programming Finished **

** Verify Started **

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000002e msp: 0x20005000

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000002e msp: 0x20005000

verified 35012 bytes in 0.204641s (167.080 KiB/s)

** Verified OK **

** Resetting Target **

adapter speed: 240 kHz

shutdown command invoked

What I see on board is 4 LEDs blinking all the time. If I am not wrong, the PingPong example should send the PING message directly and just turn on the blue LED. However, when I use a UART terminal, this is what I see (in a loop):

0690X0000060RnHQAU.pngThe PING message is not shown (I assume that the board is not even transmitting). When I try to debug the program to investigate the problem I get this error:

0690X0000060RnvQAE.png

I am working with a virtual machine with Windows 10 as host. I updated the ST-Link to the latest version and I am just using one B-L072Z-LRWAN1 board to verify that it transmits a message.

Does anyone have an idea of what is happenning?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

You need to make sure not to enable Low Power mode for the build, as this will result in debugger disconnection. Make sure you have the define LOW_POWER_DISABLE

Sorry not using Eclipse or OpenOCD tools

The DISCO board has it's own Ping-Pong build, the examples worked in Keil as I recall, but you might have to adjust the project options/defines to reflect the Radio Band used in your jurisdiction. And the frequencies, bands, and radio settings would need to be coherent across all nodes.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

You need to make sure not to enable Low Power mode for the build, as this will result in debugger disconnection. Make sure you have the define LOW_POWER_DISABLE

Sorry not using Eclipse or OpenOCD tools

The DISCO board has it's own Ping-Pong build, the examples worked in Keil as I recall, but you might have to adjust the project options/defines to reflect the Radio Band used in your jurisdiction. And the frequencies, bands, and radio settings would need to be coherent across all nodes.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
pbdiazam
Associate II

I did it adding '#define DEBUG' in the debug.c file so the debug is enabled for different modes:

void DBG_Init(void)

{

#ifdef DEBUG

 GPIO_InitTypeDef gpioinitstruct = {0};

  

 /* Enable the GPIO_B Clock */

 __HAL_RCC_GPIOB_CLK_ENABLE();

 /* Configure the GPIO pin */  

 gpioinitstruct.Mode  = GPIO_MODE_OUTPUT_PP;

 gpioinitstruct.Pull  = GPIO_PULLUP;

 gpioinitstruct.Speed = GPIO_SPEED_HIGH;

  

 gpioinitstruct.Pin  = (GPIO_PIN_12 | GPIO_PIN_13| GPIO_PIN_14 | GPIO_PIN_15);

 HAL_GPIO_Init(GPIOB, &gpioinitstruct);

 /* Reset debug Pins */

 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_RESET);

 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_13, GPIO_PIN_RESET);

 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14, GPIO_PIN_RESET);

 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_15, GPIO_PIN_RESET);

 __HAL_RCC_DBGMCU_CLK_ENABLE( );

 HAL_DBGMCU_EnableDBGSleepMode( );

 HAL_DBGMCU_EnableDBGStopMode( );

 HAL_DBGMCU_EnableDBGStandbyMode( );

  

#else /* DEBUG */

 /* sw interface off*/

 GPIO_InitTypeDef GPIO_InitStructure ={0};

  

 GPIO_InitStructure.Mode  = GPIO_MODE_ANALOG;

 GPIO_InitStructure.Pull  = GPIO_NOPULL;

 GPIO_InitStructure.Pin  = (GPIO_PIN_13 | GPIO_PIN_14);

 __GPIOA_CLK_ENABLE() ;  

 HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);

 __GPIOA_CLK_DISABLE() ;

  

 __HAL_RCC_DBGMCU_CLK_ENABLE( );

 HAL_DBGMCU_DisableDBGSleepMode( );

 HAL_DBGMCU_DisableDBGStopMode( );

 HAL_DBGMCU_DisableDBGStandbyMode( );

 __HAL_RCC_DBGMCU_CLK_DISABLE( );

#endif

}

Thank you so much! The debugger is working now.