2014-03-27 8:35 PM
Hi,
In brief, sample code appears to set Scale 3 VOS setting, but datasheet tells to set Scale 2. Who is wrong? I am running ''Demonstration'' project from stsw-stm32136.zip on STMF401 discovery board I noticed that file STM32F401-Discovery_FW_V1.0.0\Projects\Demonstration\system_stm32f4xx.c has lines: /* Select regulator voltage output Scale 2 mode, System frequency up to 84 MHz */ ... PWR->CR &= (uint32_t)~(PWR_CR_VOS); In the debugger I see that after reset PWR_CR was 0x8000, but the above line changes it to 0x4000 and it remains 0x4000 for the duration of application execution. But STM32F401xB/C Reference manual says Bits15:14 VOS[1:0]: 00: Reserved (Scale 3 mode selected) 01: Scale 3 mode 10: Scale 2 mode 11: Reserved (Scale 2 mode selected) Also, STM32F401xC datasheet says Scale 3 for fHCLK ≤ 60 MHz Scale 2 for 60 MHz < fHCLK ≤ 84 MHz So, after reset MCU had PWR_CR 0x8000 - Scale 2. This is correct:MCU can run up to max speed of 84 MHz. But that strange line PWR->CR &= (uint32_t)~(PWR_CR_VOS); erased PWR_CR to 0x4000 - Scale 3 which can only run up to 60 MHz, but the same system_stm32f4xx.c configures HCLK for 84 MHz. So, there is an error somewhere - either in the datasheet, reference manual or source code. So, the first question: where is the error? Second: what is the correct setting for VOS on STMF401 at 84 MHz? Third: what happens if the wrong VOS is selected? Will it run incorrectly? Will power consumption be bad? Will any damage happen? Thank you