Skip to main content
martonmiklos
Senior
September 13, 2017
Solved

[CubeMX regression]Failed to generate code with 4.22.1

  • September 13, 2017
  • 1 reply
  • 662 views
Posted on September 13, 2017 at 08:46

The new CubeMX 4.22.1 fails to generate code (and hangs on generation) for a STM32 workbench project which has been successfully generated with the previous versions.

Here is the command line output from the problem:

https://pastebin.com/kgumCq6t

 

I am using Linux please see the ioc file attached. The error also occurs when generating blank project.

#bug #regression #cubemx-4.22
This topic has been closed for replies.
Best answer by martonmiklos
Posted on September 15, 2017 at 13:12

This issue only happened with an updated 4.22.1 CubeMX. After reinstallation it works fine.

1 reply

martonmiklos
martonmiklosAuthorBest answer
Senior
September 15, 2017
Posted on September 15, 2017 at 13:12

This issue only happened with an updated 4.22.1 CubeMX. After reinstallation it works fine.