cancel
Showing results for 
Search instead for 
Did you mean: 

Programming Flash with JTAG - Not enough information

dhiller
Associate II
Posted on September 21, 2009 at 08:47

Programming Flash with JTAG - Not enough information

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
sjo
Associate II
Posted on May 17, 2011 at 13:21

Have a look at openocd, it already implements the jtag layer and has support for programming stm32 micros.

http://openocd.berlios.de

Cheers

sjo

dhiller
Associate II
Posted on May 17, 2011 at 13:21

I have STM32F103VC and VD devices. I need to develop a model for an in-circuit tester that will program the flash through the JTAG port.

I have the Flash Programming Manual PM0042, that shows me all of the FPEC registers and flow charts that show me the programming and erase procedures. I have the Reference Manual RM0008 that describes the JTAG port and its 2 TAP controllers and how to access them.

There does not seem to be enough information that will show me how to access the FPEC registers with the JTAG, and program/read-back the flash with the JTAG. Where is this documented?

ahnniu
Associate II
Posted on May 17, 2011 at 13:21

Hi Dudley:

Here are some information you might need to:

1. Cortex-M3 Technical Reference Manual:

http://infocenter.arm.com/help/topic/com.arm.doc.ddi0337e/DDI0337E_cortex_m3_r1p1_trm.pdf

.

You can refer to the chapter 10--Core Debug,chapter 11--System Debug,chapter 12--Debug Port.

2. ARM Debug Interface v5 Architecture Specification:

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ihi0031a/index.html

3. If you have installed Keil MDK, you will find ready-made Flash programming algorithm on \Keil\ARM\Flash\STM32F10x, this source may help you.

4. You can visit

http://www.coocox.org

for more information,there is an open emluator for ARM Cortex M3--CooCox Colink, which may help you.

-----------

http://www.coocox.org

, Cooperate on Cortex, open emluator and open RTOS for Cortex M3.

dhiller
Associate II
Posted on May 17, 2011 at 13:21

No help

Your Flash Programming manual says:

''

The in-circuit programming (ICP) method is used to update the entire contents of the

Flash memory, using the JTAG, SWD protocol or the bootloader to load the user application

into the microcontroller. ICP offers quick and efficient design iterations and eliminates

unnecessary package handling or socketing of devices.''

But no other document gives me any clue whatsoever about how to do it.

Do you have anything similar to the TI document that I just attached?

Dudley

Posted on May 17, 2011 at 13:21

Hello Dudley,

if you need to program via JTAG the STM32F103VC at the in-circuit tester I would suggest to consider FlashRunner the production in-circuit programmer from SMH.

FlashRunner easily integrates into a tester and is a fast programming tool.

You can find out more at www.smh-tech.com.

Regards.

[ This message was edited by: paolo.dalben on 21-09-2009 12:18 ]