2015-03-17 05:23 AM
Hello,
I've an application that need the reading of 8 ADC channels...I had thought use DMA in order to collect a big amount of data and then calc the average.Everything works great! However, sometimes, in an aleatory way, the code crashes! :-(Any suspicion?Here is my configuration:#define NSAMPLES 35#define NUM_CHANNELS 8#define DMA_BUFFER_SIZE (NSAMPLES*NUM_CHANNELS)void ADC_Configuration(void){ ADC_InitTypeDef ADC_InitStructure; ADC_CommonInitTypeDef ADC_CommonInitStructure; DMA_InitTypeDef DMA_InitStructure; /* Enable peripheral clocks *************************************************/ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE); NO init params RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); /* DMA2_Stream0 channel0 configuration **************************************/ DMA_DeInit(DMA2_Stream0); DMA_InitStructure.DMA_Channel = DMA_Channel_0; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&(ADC1->DR); DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)ADC1_Buff; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = DMA_BUFFER_SIZE; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA2_Stream0, &DMA_InitStructure); /* DMA2_Stream0 enable */ DMA_Cmd(DMA2_Stream0, ENABLE); /* Configure ADC1 Channels pins as analog input ******************************/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 ; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_4; GPIO_Init(GPIOC, &GPIO_InitStructure); /* ADC Common Init **********************************************************/ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;ADC_CommonInit(&ADC_CommonInitStructure); /* ADC1 Init ****************************************************************/ADC_Cmd(ADC1, DISABLE);ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;ADC_InitStructure.ADC_ScanConvMode = ENABLE;ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;ADC_InitStructure.ADC_NbrOfConversion = NUM_CHANNELS;ADC_InitStructure.ADC_ExternalTrigConv = 0x00;ADC_Init(ADC1, &ADC_InitStructure); /* Enable ADC1 DMA */ADC_DMACmd(ADC1, ENABLE);ADC_RegularChannelConfig(ADC1, ADC_Channel_3 , 1, ADC_SampleTime_480Cycles); ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 2, ADC_SampleTime_480Cycles); ADC_RegularChannelConfig(ADC1, ADC_Channel_2 , 3, ADC_SampleTime_480Cycles); ADC_RegularChannelConfig(ADC1, ADC_Channel_6 , 4, ADC_SampleTime_480Cycles); ADC_RegularChannelConfig(ADC1, ADC_Channel_5 , 5, ADC_SampleTime_480Cycles); ADC_RegularChannelConfig(ADC1, ADC_Channel_4 , 6, ADC_SampleTime_480Cycles); ADC_RegularChannelConfig(ADC1, ADC_Channel_10, 7, ADC_SampleTime_480Cycles); ADC_RegularChannelConfig(ADC1, ADC_Channel_14, 8, ADC_SampleTime_480Cycles); /* Enable DMA request after last transfer (Single-ADC mode) */ ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE); ADC_ContinuousModeCmd(ADC1, ENABLE); /* Enable ADC1 **************************************************************/ ADC_Cmd(ADC1, ENABLE); Delay_ms(100); /* Start ADC1 Software Conversion */ ADC_SoftwareStartConv(ADC1);}Thanks in advance!Best regards,--Guilherme2015-03-17 08:33 AM
Everything works great! However, sometimes, in an aleatory way, the code crashes! :-(
Any suspicion?Random crashes, probably not this code. Check you have adequate stack, and try to provide more information on what a ''crash'' means in this context. Where does the processor go if you stop execution? Is it in the Hard Fault handler?You'll need to get a lot more specific on what happens to understand why it happens.