2017-10-19 7:29 AM
Hi,
I'm trying to create a project using CubeMX which will use SPI1 with DMA. Unfortunately the SPI HAL driver seems to lock up after a few milliseconds of transactions (about 40 slave transactions). I see
Lock = HAL_UNLOCKED, State = HAL_SPI_STATE_BUSY_TX_RX, ErrorCode = 0
and the state never clears.
Can anyone offer any advice on what could cause this sort of lock up?
2017-10-19 7:32 AM
some further information, I call the HAL using
HAL_SPI_TransmitReceive_DMA(&hspi1, LSM6DSL_Read_Bytes, rawbuff, LSM6DSL_Read_Transaction);
but at the point of failure the state is still busy even though the callback function from the previous transaction has been called.