cancel
Showing results for 
Search instead for 
Did you mean: 

community.st.com

Philipp Krause
Senior II
Posted on January 09, 2018 at 14:06

3rd Feb talk on The free toolchain for the STM8 at FOSDEM in Brussels

At FOSDEM 2018, there will be a talk on 'The free toolchain for the STM8' in the 'Embedded, mobile and automotive devroom'.

The talk in the will be 2018-02-03 11:00 in room UD2.218A at the Universit� libre de Bruxelles.

There has been a lot of recent progress, from the speed optimizations in SDCC to the on-target-debugging support via OpenOCD and GDB.

I will also be around for discussions during that weekend.

More details on the talk can be found at:

https://community.st.com/external-link.jspa?url=https%3A%2F%2Ffosdem.org%2F2018%2Fschedule%2Fevent%2Fthe_free_toolchain_for_the_stm8%2F

Philipp

#sdcc #open-source #openocd #stm8 #free-software #fosdem
0 REPLIES 0