Get ready for the STM32 Summit 2026 | Online, November 3
Read our guidelines, share your thoughts about your community experience, and explore community insights.
Most recent activity
I've seen it a couple of times - both from ST Employees, IIRC; eg,https://community.st.com/t5/mems-sensors/lsm6dso-and-lsm6dso32-compatible/m-p/891941/highlight/true#M27029 Neither the button nor the option allows just formatting a single word like that. Looking at the HTML view of the above post, it's using the <code> tag - but I don't see any way to enter that via the Editor?(I did that one via the HTML editor - but that's very klunky!)
Tried to paste code in reply. Noticed, that line count does not match. Clicked in editor and it started to duplicate.Also check out attached video.In order to reproduce the bug, longer code must be pasted in C code insert tool from tool bar. Then mouse pointer must be navigated at the end of inserted code and clicked few times here and there. Inserted code will start to duplicate in editor.
For the past week or so, pasting images directly into posts seems to have broken.I used to be able to just take a screenshot, or copy an image and paste it straight into the editor, but that no longer works.I press 'paste', and nothing happens - no error messages or anything.I am now having to save the image locally, and then use the 'Insert Photos' button to import it. There is history with this, but now it seems to have just broken completely. Using Chrome Version 145.0.7632.109 (Official Build) (64-bit) on Windows-11 Pro
Between Last Day to Last Year, doesn't show users. Only All Time shows users.
144 characters
Or 'Feature Request' or similar.Applies to CubeIDE, CubeMX, and CubeMX2 - probably also others ...eg, see here and here.
My post was deleted without any notification or reason? https://community.st.com/t5/escalated-topic/stm32h5-fdcan-system-bootloader/m-p/886189#M30060
so it seems:https://community.st.com/t5/stm32-mcus-embedded-software/sd-card-no-file-system-error/m-p/641421/highlight/true#M45513On other forums, the 'Mark As Solution' just changes to 'Unmark Solution' (or whatever) - so it's always obvious, and in the same place. Addendum:Perhaps this: https://community.st.com/t5/stm32-mcus-embedded-software/sd-card-no-file-system-error/m-p/641422/highlight/true#M45514 could be added here: https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256
Currently, questions are going in the Interface and connectivity ICs forum, but there don't seem to be any suitable labels:I don't think 'Low Power RF Solutions' really covers it?The Product Page on the main website comes under 'Wireless connectivity > Long range > NB-IoT products':So I guess that would be a good set of labels?
I'm trying to reply to a post. I'm logged in. I typed a response and attached an image with the "Insert Photos" tool. After hitting Reply, I see the message "An Unexpected Error has occurred". I've seen this a few times over the past week but didn't both posting this bug report until now.Anyone else?
When writing a reply, if the message includes images, parts of the post can be deleted after pressing the "Reply" button. This has happened many times over the last week. Since the data is deleted, there is no way to recover but to edit and re-enter that information.This is a big waste of time. Why is the forum software getting worse?
Since ~2 hours I get thousands of mails from notification@communitymailer.st.com mainly with STM8 stuff from the last years.What's going wrong here? Is it only me? I never was interested in STM8, just STM32...(I unsubscribed from "others: hardware and software" to survive the day.) P.S.: they all have the same init line like this:Hi mfgkw, Lina_DABASINSKAITE (Community manager) moved a topic in Others: hardware and software on 2020-09-08 8:15 AM: Where can I get the stm8s discovery dev.zip file? I would like to download the application code that is advertised with the eval/demo board but can't find it anywhere on ST.com. Thanks. They all seem to start with "Lina_DABASINSKAITE (Community manager) moved a topic in Others: hardware and software on " ...
See:User authentication service maintenance on 26 February (CubeIDE forum);User authentication service maintenance on 26 February (CubeMX forum).Neither of these says what time the maintenance is scheduled to occur. Temporary Unavailability of Server Update Pack – Maintenance on February 26 (in the VSCode forum) does give a time, but no timezone.
On some post now I get an errorHave been on this forum for 8 years or so, never had this issue..I tried to report a fix to someone, can't do that.. This is a great way to block uses reporting solutions.What is this ? Cannot find any link how to verify.Please help ASAPI also don't see Sidekick on any forum, is that related ?
In all the areas which currently have labels for the other peripherals. See: STM32H5E4/E5/F4/F5 with PLAY: boards availability?.
The current marking is one character per line and it bleeds into other posts. Looks very amateur. The new forum has been here for many years at this point, can we improve the presentation here?
Hi,When I posted a question, the following warning message appeared on the post:Marked as spam.This is the URL for my post.https://community.st.com/t5/stm32-mpus-embedded-software-and/sd-card-read-issue/m-p/881342#M5615This post doesn't appear on the forum board and can't be found through searches...Best Regards,Karsten
See: STM32CubeMX 6.17.0 released by @Aimen1 The link to Getting started with Programmable Logic ArraY (PLAY) - stm32mcu is wrong:Link is: https://wiki.st.com/stm32mcu/wiki/Getting_started_with_Programmable_Logic_ArraYshould be: https://wiki.st.com/stm32mcu/wiki/Getting_started_with_Programmable_Logic_ArrayBut even with the correct link, the page is empty: And why is the URL case-sensitive anyhow? PS:In fact, there seems to be no information at all about this anywhere - see: So what's all this "PLAY (Programmable Logic Array) on STM32H5 4M" stuff, then ?
eg, here: It often seems to be used by "accident" by beginners.In this case possibly because, in the "extended" toolbar, it's in the place where 'insert image' was on the "basic" toolbar:
Hi,Using Safari 26.2 I'm unable to delete or edit my own posts. Does anyone else
The conversation window with the company's chatbot exhibits a glitch.Specific manifestation: The window flickers when inactive.Trigger method: After posing a question and receiving the AI's response, scroll down to the bottom of the conversation window using the mouse wheel immediately after the reply concludes to reproduce the bug. (This has only occurred once thus far; subsequent testing failed to replicate the issue.)The ST Community moderator has edited the post to comply with the ST Community language: English. For more information, see: ST Community Terms and Conditions.Translated with DeepL.com (free version)
See:https://community.st.com/t5/stm32-mcus-boards-and-hardware/struggling-with-a-simple-uart-printf-on-nucleo-g474re-works-on/m-p/874056/highlight/true#M29428 Sidekick says UART2, but the User Manual & Schematics show LPUART1 (default) or UART1 (by changing solder bridges):UM screenshot: https://community.st.com/t5/stm32-mcus-boards-and-hardware/struggling-with-a-simple-uart-printf-on-nucleo-g474re-works-on/m-p/874047/highlight/true#M29425Schematic screenshots - by @mƎALLEm:https://community.st.com/t5/stm32-mcus-boards-and-hardware/struggling-with-a-simple-uart-printf-on-nucleo-g474re-works-on/m-p/874051/highlight/true#M29427
It's been sat there "thinking" for several minutes now!Just putting "NUCLEO-G474RE VCP" did get an answer
Welcome to the ST Community highlights for October to December 2025. This quarter, we introduced you to STM32 Sidekick: AI-powered tool, trained exclusively on official STM32 documentation, and helps you find answers quickly. Log in to start using STM32 Sidekick.Now, let's review the latest achievements and the most active areas in the ST Community from this period.Top 3 community members who authored the most solutions: @TDK with 105 solutions authored. @Andrew Neil with 39 solutions authored. @Issamos with 35 solutions authored. Top 3 most viewed solutions: Solved: Re: CubeIDE 2.0 does not open .ioc files authored by @Andrew Neil. Solved: Re: STM32CubeIDE 2.0 detached STM32CubeMX problem authored by @JensH. Solved: Re: Any small tutorial for the STM32CubeIDE v2.0.0 ? authored by @mfgkw. Top 3 most viewed knowledge base articles STM32CubeIDE 2.0.0 workflow tutorial authored by @ST AME Support NF. How to implement an air b
Hello, I can't download any software from this, I mean st.com. After popup with License Agreement download doesn't start. I am only one with this issue? Problem occurs on Mozilla Firefox. On Chrome it works fine.
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.