Skip to main content
TDK
Mar 4, 2026 3:22 PM UTC
Question

Parts of a reply are deleted when hitting Reply

When writing a reply, if the message includes images, parts of the post can be deleted after pressing the "Reply" button. This has happened many times over the last week. Since the data is deleted, there is no way to recover but to edit and re-enter that information.

This is a big waste of time. Why is the forum software getting worse?

9 replies

TDK
TDKAuthor
Mar 4, 2026 3:23 PM UTC

This is the first line of my reply.

 

Here is a random image:

Screenshot 2026-03-04 102259.png

And here is the rest of my reply.

 

Edit: trying to get the bug to occur so I can document it.

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
TDKAuthor
Mar 4, 2026 3:25 PM UTC

deleted, bug didn't occur

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
Mar 4, 2026 3:24 PM UTC

Is this after a failed attempt to paste an image?

We know that Pasting images not working.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Mar 4, 2026 3:27 PM UTC

A Test.

I will now try to paste an image:

 

It didn't work, of course!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Mar 4, 2026 3:34 PM UTC

@Andrew Neil wrote:

A Test.

I will now try to paste an image:

 

It didn't work, of course!


But the whole message did post (less the image, of course).

Looking at the HTML before posting:

Image2.png

We can see where the image should be.

When I pressed the button to actually post the reply, I got the dreaded "HTML error":

Image1.png

@TDK  I suspect that something goes wrong with whatever "changes" that does to "correct" the "error" - which causes loss of some of your post?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
TDKAuthor
Mar 7, 2026 2:36 PM UTC

Here's a post where it ate the image that I inserted with the Insert Photos button. I suspect it would have also eaten any text I sent after the image.

Before posting:

Screenshot 2026-03-07 093328.png

And the post (I edited it to add the image back in):

Screenshot 2026-03-07 093600.png

 

configure SPSB081 watchdog - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."
Lina_DABASINSKAITE
ST Community Manager
Mar 9, 2026 2:49 PM UTC

Thanks for providing this @TDK. I am passing this to troubleshooting team. 

Regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.