Skip to main content
Andrew Neil
Super User
Apr 13, 2026 2:20 PM UTC
Question

What's this new character-level 'code' format?

I've seen it a couple of times - both from ST Employees, IIRC; eg,

AndrewNeil_1-1776089549905.png

https://community.st.com/t5/mems-sensors/lsm6dso-and-lsm6dso32-compatible/m-p/891941/highlight/true#M27029

 

Neither the AndrewNeil_2-1776089605906.png button nor the AndrewNeil_3-1776089630142.pngoption allows just formatting a single word like that.

 

Looking at the HTML view of the above post, it's using the <code> tag - but I don't see any way to enter that via the Editor?

(I did that one via the HTML editor - but that's very klunky!)

2 replies

Andrew Neil
Super User
Apr 13, 2026 2:24 PM UTC

@Andrew Neil wrote:

ither the AndrewNeil_2-1776089605906.png button nor the AndrewNeil_3-1776089630142.pngoption allows just formatting a single word like that.

 

Looking at the HTML view of the above post, it's using the <code> tag - but I don't see any way to enter that via the Editor?


That appeared correctly in the editor, but broke on posting:

AndrewNeil_0-1776090237145.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Peter BENSCH
ST Technical Moderator
Apr 13, 2026 3:35 PM UTC

This type of formatting occurs when someone pastes pre-formatted text – for example, from ChatGPT – using a simple copy-and-paste, thereby copying its formatting. To prevent this, you can paste such text as plain ASCII text by using Ctrl+Shift+V instead of Ctrl+V.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.