Skip to main content
debugging
Lead
Feb 15, 2026 2:43 AM UTC
Solved

How to verify email address ?

On some post now I get an error

debugging_0-1771125006604.png

Have been on this forum for 8 years or so, never had this issue..

I tried to report a fix to someone, can't do that.. This is a great way to block uses reporting solutions.

What is this ? Cannot find any link how to verify.

Please help ASAP

I also don't see Sidekick on any forum, is that related ?

 

Lina_DABASINSKAITE
ST Community Manager
Mar 4, 2026 12:38 PM UTC

Hi @debugging,

The team has implemented the necessary changes for the second point. The text that appears when hovering over the chatbot now states: Open STM32 Sidekick.

 
 

Screenshot 2026-03-04 133645.png

Thank you for highlighting this point. 
Lina 

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

7 replies

TDK
Feb 16, 2026 5:19 AM UTC

> On some post

The post is likely read only, as the message suggests. Perhaps provide a link. You're clearly able to interact with the forum by making this post.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Lina_DABASINSKAITE
ST Community Manager
Feb 17, 2026 8:52 AM UTC

Hi @debugging, 

To confirm what @TDK said. This text appears for read-only threads, and you are logged out. If it's not the case, please send over a screenshot and URL where it does appear to you. 

As for the Sidekick, it's working and should appear on Welcome page and on all STM32 MCUs and STM32 MPUs related forum boards. Share a screenshot where it does not appear to you. 

Regards,
Lina 

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
debugging
debuggingAuthor
Lead
Feb 19, 2026 1:32 PM UTC

thanks for the reply.

1. Yes I was logged in and Yes the thread was locked/read only.  I was  wondering i needed to verify  my email address or how I could see my email is "verified" or not and there wasn't a verify option in my profile. As I was logged in perhaps the error message could be more intelligent.

2. I understand now that "sidekick" is the icon. when I moved my mouse over the icon it said "open chat" . I could not find the word "sidekick" in any of the webpages so wondered what or where it was.

debugging_0-1771507270847.png

3.  I am not sure why I see the icon it now. perhaps related to https://community.st.com/t5/feedback-forum/having-issue-with-stm32-sidekick-with-firefox/m-p/865804  but I use Ubuntu with Firefox.

 

 

 

Lina_DABASINSKAITE
ST Community Manager
Mar 2, 2026 4:44 PM UTC

Hi @debugging, 

Thanks for additional information. 

For the 1st point - I am checking if the notification message can vary based on the log-in status. If not, we will have to keep it as it is. 

For 2nd - I have passed the feedback to the respective team. I will let you now once there are news on this. 

Regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Mar 2, 2026 5:01 PM UTC

@Lina_DABASINSKAITE wrote:

I am checking if the notification message can vary based on the log-in status.


It seems to be the standard message - example screenshots here and here.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.