2017-07-21 6:49 AM
Hi all :
I am using the STM32L4xx Stm Cube drivers for AES-256 ECB encryption on the STM32L4 Although the encrypted data comes out perfectly, the decrypted encrypted data is not the original plaintext. To be clear: I am not using the X crypto library, but instead the
and modules that are included in the from the STM Cube STM32L4xx HAL Drivers.Some info about the code:
-The MX_AES_Init function uses
HAL_CRYP_Init to initialize the AESmodule
- I am using this API to encrypt and decrypt data:
HAL_CRYP_AESECB_Encrypt_IT
-After the encryption, I deinit the AES module change the operating mode to decrypt and re init using the HAL init function
- I tried setting the original operating mode to decrypt and feeding in the encrypted output, but I get the same incorrect decrypted data instead of the original plaintext I added .
When I try to decrypt the cipher_text array back to the plain_text array it doesn't work, but the encrypted data is correct according to
http://www.cryptogrium.com/aes-encryption-online-ecb.html
.uint8_t plain_text[64] =
{ 0x6b, 0xc1, 0xbe, 0xe2, 0x2e, 0x40, 0x9f, 0x96, 0xe9, 0x3d, 0x7e, 0x11, 0x73, 0x93, 0x17, 0x2a, 0xae, 0x2d, 0x8a, 0x57, 0x1e, 0x03, 0xac, 0x9c, 0x9e, 0xb7, 0x6f, 0xac, 0x45, 0xaf, 0x8e, 0x51, 0x30, 0xc8, 0x1c, 0x46, 0xa3, 0x5c, 0xe4, 0x11, 0xe5, 0xfb, 0xc1, 0x19, 0x1a, 0x0a, 0x52, 0xef, 0xf6, 0x9f, 0x24, 0x45, 0xdf, 0x4f, 0x9b, 0x17, 0xad, 0x2b, 0x41, 0x7b, 0xe6, 0x6c, 0x37, 0x10 };uint8_t Key[32] =
{ 0x60, 0x3d, 0xeb, 0x10, 0x15, 0xca, 0x71, 0xbe, 0x2b, 0x73, 0xae, 0xf0, 0x85, 0x7d, 0x77, 0x81, 0x1f, 0x35, 0x2c, 0x07, 0x3b, 0x61, 0x08, 0xd7, 0x2d, 0x98, 0x10, 0xa3, 0x09, 0x14, 0xdf, 0xf4, };const uint8_t ciphertext[64] =
{ 0xf3, 0xee, 0xd1, 0xbd, 0xb5, 0xd2, 0xa0, 0x3c, 0x06, 0x4b, 0x5a, 0x7e, 0x3d, 0xb1, 0x81, 0xf8, 0x59, 0x1c, 0xcb, 0x10, 0xd4, 0x10, 0xed, 0x26, 0xdc, 0x5b, 0xa7, 0x4a, 0x31, 0x36, 0x28, 0x70, 0xb6, 0xed, 0x21, 0xb9, 0x9c, 0xa6, 0xf4, 0xf9, 0xf1, 0x53, 0xe7, 0xb1, 0xbe, 0xaf, 0xed, 0x1d, 0x23, 0x30, 0x4b, 0x7a, 0x39, 0xf9, 0xf3, 0xff, 0x06, 0x7d, 0x8d, 0x8f, 0x9e, 0x24, 0xec, 0xc7 };Not sure what to do next....Thanks in advance for any help.##
#aes #encryption #crypto-aes-encrypt-stm32 #stm32l486 #crypto-aes-decrypt #aes-256 Note: this post was migrated and contained many threaded conversations, some content may be missing.Solved! Go to Solution.
2017-08-02 10:02 AM
Hi
,Tests are made on an STM32L486 device using the same configuration as yours and the decryption process worked as expected.
I attach to this post the code used for our test. Could you please use it and let us know the result?
It will be interesting also to share your .ioc file + your updated main.c file.
This should help us to do further checks.
-Amel
________________ Attachments : main_ecb.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HySk&d=%2Fa%2F0X0000000b9B%2F1HAi5wE7NFyS.KFUua7Sb43QFIRDfWhY0WiSUK_Tt6E&asPdf=falseTo give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-07-22 6:37 PM
Data does appear to be correct for AES-ECB, I don't have an STM32L486 to tinker with. Perhaps you can create a free-standing example that compiles?
2017-07-23 12:44 PM
Hi Clive One -
I did try a free standing example with an array of the encrypted data and the key from above and I get the same incorrect decrypted data. I went as far as to look at the data in memory in both builds and even there it is incorrect (but always the same incorrect decrypted data). This makes me feel like theres a bug in the drivers? Or maybe I need to do something with the decrypted data after running the API function?? But that doesn't make sense to me either.
Thanks for the help.
-Jennifer
2017-07-23 1:35 PM
It's hard for me to debug remotely and blind, if the API was a complete bust for encrypt-decrypt cycle then I suspect to see a lot more forum traffic. That said the chips with the encryption engine have a much more limited user base. The AES engine in the F215 performed quite robustly. One would hope that ST did at least some minimal functional testing of the library/API.
2017-07-23 1:44 PM
One of the Cube examples should port and validate the engine
STM32Cube_FW_L4_V1.8.0\Projects\STM32L496ZG-Nucleo\Examples\CRYP\CRYP_AESModes\Src\main.c
2017-07-26 1:42 PM
DAHMEN.IMEN
 Could you help me with this?2017-07-26 2:51 PM
Hi Clive One -
That is actually legacy code according to the code I generated in MX Cube. Although my code has the same procedure only using the new API (which only has one function for decryption and encryption).
Th behavior using both APIs is strange. The encryption is working but I am still not getting the original plaintext back during the decryption
:(
Jennifer
2017-07-26 3:05 PM
Get an
STM32L486 board on my desk, I'll take a look at this.
2017-07-26 3:36 PM
Get or got?
2017-07-26 3:39 PM
Get