2018-01-22 6:59 PM
I want to add crc function for the IAP-APP function. So I used the CRC example inSTM32Cube_FW_F0_V1.9.0 to test. But
uwCRCValue
is always 0. I think theuwExpectedCRCValue
should be the last four byte (0x0803FFFB-0x0803FFFF
), anduwCRCValue
should be the same value. Attach is the IAR configuration for CRC. Did my understanding wrong or my code below is wrong?#define BUFFER_SIZE 114
static const uint32_t aDataBuffer[BUFFER_SIZE]
#ifdef PUBLIC_C = { 0x00001021, 0x20423063, 0x408450a5, 0x60c670e7, 0x9129a14a, 0xb16bc18c, 0xd1ade1ce, 0xf1ef1231, 0x32732252, 0x52b54294, 0x72f762d6, 0x93398318, 0xa35ad3bd, 0xc39cf3ff, 0xe3de2462, 0x34430420, 0x64e674c7, 0x44a45485, 0xa56ab54b, 0x85289509, 0xf5cfc5ac, 0xd58d3653, 0x26721611, 0x063076d7, 0x569546b4, 0xb75ba77a, 0x97198738, 0xf7dfe7fe, 0xc7bc48c4, 0x58e56886, 0x78a70840, 0x18612802, 0xc9ccd9ed, 0xe98ef9af, 0x89489969, 0xa90ab92b, 0x4ad47ab7, 0x6a961a71, 0x0a503a33, 0x2a12dbfd, 0xfbbfeb9e, 0x9b798b58, 0xbb3bab1a, 0x6ca67c87, 0x5cc52c22, 0x3c030c60, 0x1c41edae, 0xfd8fcdec, 0xad2abd0b, 0x8d689d49, 0x7e976eb6, 0x5ed54ef4, 0x2e321e51, 0x0e70ff9f, 0xefbedfdd, 0xcffcbf1b, 0x9f598f78, 0x918881a9, 0xb1caa1eb, 0xd10cc12d, 0xe16f1080, 0x00a130c2, 0x20e35004, 0x40257046, 0x83b99398, 0xa3fbb3da, 0xc33dd31c, 0xe37ff35e, 0x129022f3, 0x32d24235, 0x52146277, 0x7256b5ea, 0x95a88589, 0xf56ee54f, 0xd52cc50d, 0x34e224c3, 0x04817466, 0x64475424, 0x4405a7db, 0xb7fa8799, 0xe75ff77e, 0xc71dd73c, 0x26d336f2, 0x069116b0, 0x76764615, 0x5634d94c, 0xc96df90e, 0xe92f99c8, 0xb98aa9ab, 0x58444865, 0x78066827, 0x18c008e1, 0x28a3cb7d, 0xdb5ceb3f, 0xfb1e8bf9, 0x9bd8abbb, 0x4a755a54, 0x6a377a16, 0x0af11ad0, 0x2ab33a92, 0xed0fdd6c, 0xcd4dbdaa, 0xad8b9de8, 0x8dc97c26, 0x5c644c45, 0x3ca22c83, 0x1ce00cc1, 0xef1fff3e, 0xdf7caf9b, 0xbfba8fd9, 0x9ff86e17, 0x7e364e55, 0x2e933eb2, 0x0ed11ef0 } #endif ;static void MX_CRC_Init(void)
{ CrcHandle.Instance = CRC;/* The default polynomial is not used. It is required to defined it in CrcHandle.Init.GeneratingPolynomial*/
CrcHandle.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;/* Set the value of the polynomial */
//CrcHandle.Init.GeneratingPolynomial = DEFAULT_POLYNOMIAL_ENABLE;/* The size of the polynomial to configure the IP is 8b*/
CrcHandle.Init.CRCLength = CRC_POLYLENGTH_32B;/* The default init value is used */
CrcHandle.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_DISABLE;/* The input data are not inverted */
CrcHandle.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;/* The output data are not inverted */
CrcHandle.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;/* The input data are 32 bits lenght */
CrcHandle.InputDataFormat = CRC_INPUTDATA_FORMAT_WORDS;if (HAL_CRC_Init(&CrcHandle) != HAL_OK)
{ /* Initialization Error */ Error_Handler(); }}
void APP_CRC(void)
{ /*##-2- Compute the CRC of 'aDataBuffer' ###################################*/ uwCRCValue = HAL_CRC_Calculate(&CrcHandle, (uint32_t *)&aDataBuffer, BUFFER_SIZE); TRACE_DBG_STRING(DEBUG_MODULE, LOG_LVL_INFO, 'APP_CRC: %x,%x', uwCRCValue,uwExpectedCRCValue);/*##-3- Compare the CRC value to the Expected one ##########################*/
if (uwCRCValue != uwExpectedCRCValue) { /* Wrong CRC value: enter Error_Handler */ TRACE_DBG_STRING(DEBUG_MODULE, LOG_LVL_INFO, 'CRC err');//Error_Handler();
} else { /* Right CRC value: Turn LED2 on */ TRACE_DBG_STRING(DEBUG_MODULE, LOG_LVL_INFO, 'CRC success'); }}
Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-01-22 7:22 PM
Can't see attachments, but this code won't sum across the ROM
Make sure you enable the clock, otherwise the peripheral will return zero
/* CRC Peripheral clock enable */
__HAL_RCC_CRC_CLK_ENABLE();2018-01-22 10:17 PM
Above is the IAR for CRC configuration.
I tried
__HAL_RCC_CRC_CLK_ENABLE(); but still the same result(
uwCRCValue
is always 0
)Below is my code.
void SystemClock_Config(void)
{RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInit;/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI14|RCC_OSCILLATORTYPE_HSE |RCC_OSCILLATORTYPE_LSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.LSEState = RCC_LSE_ON; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSI14State = RCC_HSI14_ON; RCC_OscInitStruct.HSI14CalibrationValue = 16; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL3; RCC_OscInitStruct.PLL.PREDIV = RCC_PREDIV_DIV1; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); }/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{ Error_Handler(); }PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_I2C1
|RCC_PERIPHCLK_RTC; PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_SYSCLK; PeriphClkInit.I2c1ClockSelection = RCC_I2C1CLKSOURCE_SYSCLK; PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK) { Error_Handler(); }/**Configure LSE Drive Capability
*/ __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);/**Configure the Systick interrupt time
*/ HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick
*/ HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 3, 0);}static void MX_CRC_Init(void)
{ CrcHandle.Instance = CRC;/* The default polynomial is not used. It is required to defined it in CrcHandle.Init.GeneratingPolynomial*/
CrcHandle.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;/* Set the value of the polynomial */
//CrcHandle.Init.GeneratingPolynomial = DEFAULT_POLYNOMIAL_ENABLE;/* The size of the polynomial to configure the IP is 8b*/
CrcHandle.Init.CRCLength = CRC_POLYLENGTH_32B;/* The default init value is used */
CrcHandle.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_DISABLE;/* The input data are not inverted */
CrcHandle.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;/* The output data are not inverted */
CrcHandle.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;/* The input data are 32 bits lenght */
CrcHandle.InputDataFormat = CRC_INPUTDATA_FORMAT_WORDS;__HAL_RCC_CRC_CLK_ENABLE();
if (HAL_CRC_Init(&CrcHandle) != HAL_OK) { /* Initialization Error */ Error_Handler(); }}
2018-01-22 10:59 PM
I tried again. It is useful to add
__HAL_RCC_CRC_CLK_ENABLE(); , I get the
uwCRCValue
=ebf5058c, but the IAR tool add the CRC value in the bin file is 81539A62. It is not the same.2018-01-23 10:48 PM
Hi Clive, can you help me to see my below problem?
2018-01-24 1:50 AM
Can't currently see attachments and not using IAR. Assume you are summing wrong region or using wrong polynomial.
2018-01-24 4:46 PM
Fill pattern: 0xFF
Start address:0x08020000 End address:0x0803FFFB
Checksum size: 4bytes Alignment:4
Algorithm: CRC32
Complement: As is Initial value: 0xFFFFFFFF/0(I tried both
0xFFFFFFFF and 0, but crc still wrong
)Bit border: MSB first check: use as input
uncheck: reverse byte order within word
Checksum unit size: 32-byte
Above are my IAR configurations for crc
2018-01-24 5:46 PM
IAR says uncheck 'use as input'
2018-01-24 8:18 PM
It's very useful for your above answer. I think the wrong crc because of my
wrong region
,but I can't confirm. And I've tried many times for my code, I can't find where it is wrong. Please help me have a check.//init
static void MX_CRC_Init(void)
{ CrcHandle.Instance = CRC;/* The default polynomial is not used. It is required to defined it in CrcHandle.Init.GeneratingPolynomial*/
CrcHandle.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;/* Set the value of the polynomial */
//CrcHandle.Init.GeneratingPolynomial = DEFAULT_POLYNOMIAL_ENABLE;/* The size of the polynomial to configure the IP is 8b*/
CrcHandle.Init.CRCLength = CRC_POLYLENGTH_32B;/* The default init value is used */
CrcHandle.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE;/* The input data are not inverted */
CrcHandle.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;/* The output data are not inverted */
CrcHandle.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;/* The input data are 32 bits lenght */
CrcHandle.InputDataFormat = CRC_INPUTDATA_FORMAT_WORDS;__HAL_RCC_CRC_CLK_ENABLE();
if (HAL_CRC_Init(&CrcHandle) != HAL_OK) { /* Initialization Error */ Error_Handler(); }}
2018-01-24 8:23 PM
// check the crc---------------
ApplicationEndAddress = 0x0803FFFC/0x0803FFFB, I tried both these two address, but still wrong
U8 APP_CRC(void)
{U32 ApplicationStartAddress = 0x08020000;
U32 ApplicationEndAddress = 0x0803FFFC;uwCRCValue = HAL_CRC_Calculate(&CrcHandle, (uint32_t *)&ApplicationStartAddress, (ApplicationEndAddress-ApplicationStartAddress)/4);
/*♯♯-3- Compare the CRC value to the Expected one ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ if (uwCRCValue != __checksum) { /* Wrong CRC value: enter Error_Handler */ TRACE_DBG_STRING(DEBUG_MODULE, LOG_LVL_INFO, 'CRC err'); return FALSE;// Error_Handler();
} else { /* Right CRC value: Turn LED2 on */ TRACE_DBG_STRING(DEBUG_MODULE, LOG_LVL_INFO, 'CRC success'); return TRUE; }}
//IAR configuration
Fill pattern: 0xFF
Start address:0x08020000 End address:0x0803FFFB
Checksum size: 4bytes Alignment:4
Algorithm: CRC32
Complement: As is Initial value: 0xFFFFFFFF/0(I tried both
0xFFFFFFFF and 0, but crc still wrong
)Bit border: MSB first uncheck: use as input
uncheck: reverse byte order within word
Checksum unit size: 32-byte
I modified code as above, but when I call
APP_CRC(void)
, device stop run. So I tired toHAL_CRC_Calculate(&CrcHandle, (uint32_t *)&ApplicationStartAddress, 4),
when I call
APP_CRC(void)
, device is running fine, just the crc value is wrong. So I think it is because I fill the wrong len in the
HAL_CRC_Calculate
. So (ApplicationEndAddress-ApplicationStartAddress)/4 is wrong?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.