2018-03-30 7:31 AM
Hello everyone. I need to help immediately. I neet to disable VBUS pin on STM32F429. How can I do ? please help me
2018-03-30 7:38 AM
Hi
_st_n.kadir
,Unfortunately, it is difficult to follow the status of issues you are facing.
Each time a new discussion on the forum for almost the same topic (3)This is confusing...don't know where to start exactly... To be able to efficiently help you, I suggest you provide a clear status onone post!-Nesrine-
2018-03-30 9:47 AM
actually I use CAN2 at STM32F429ZI. but, ı can not connect PB13 because of VBUS. I need to disable VBUS. but, I dont know how ı can
2018-03-30 10:01 AM
>> I need to help immediately.
This isn't how forums work, for immediate help hire contractors/consultants that answer to you, and are paid
http://www.catb.org/esr/faqs/smart-questions.html
The use of PB13 VBUS is specific to the STM32F429I-DISCO board design.
Review the schematic, follow the traces, and try to determine if those can be cut or modified to meet your requirements.
2018-03-30 10:02 AM
'
ı can not connect PB13 because of VBUS.'
what does that mean?
'I need to disable VBUS. but, I dont know how ı can '
would reading the datasheet help?
2018-03-30 10:13 AM
The question is poorly framed. The OP is using the STM32F429I-DISCO where PB13 is wired as VBUS and connects to an LED, etc
2018-03-31 3:39 PM
Thank you for answered. When I look datasheet, it says you can use PB13 pin as CAN2_Tx
2018-03-31 3:40 PM
Thank you for answered
2018-04-02 6:07 AM
That is as far as the chip itself is concerned.
On the Discovery board, as
Turvey.Clive.002
has explained, the pin is used to detect the presence of VBUS.