cancel
Showing results for 
Search instead for 
Did you mean: 

Switch relay synchronously in 0 passage (50Hz)

ATürk.11
Associate II

i am trying to switch a relay via the stm8s001 processor synchronously in the 0 pass. how could I realize that.

i have an imput signal of 50 Hz. I can also start the timer, but I don't know how to switch the relay on exactly in the 0 cycle.

(i watch the action on the oscilloscope).

The Code.:

main.c .:

(only the most important areas)

##################################################################

void main(void)

{

  

CONFIG_UNUSED_PINS_STM8S001;

//STARTUP_SWIM_DELAY_5S; 

GPIO_Config();

CLK_Config();

TIMER_Config();

EXTI_SetExtIntSensitivity(EXTI_PORT_GPIOD, EXTI_SENSITIVITY_RISE_ONLY);

enableInterrupts();

while(1)

{

if (flagfortimer == 1 )

GPIO_WriteReverse(GPIOA, GPIO_PIN_3);

flagfortimer = 0;

}

}

static void TIMER_Config(void)

{

  TIM1_DeInit();

TIM1_TimeBaseInit(1, TIM1_COUNTERMODE_UP,1,0); how is the dimensioning here ???

TIM1_ITConfig(TIM1_IT_UPDATE, ENABLE);

  TIM1_Cmd(ENABLE);

}

#############################################################

interrupt_vector :

{0x82, EXTI_PORTD_IRQHandler}, /* irq6 */

.........

{0x82, TIM1_UPD_OVF_TRG_BRK_IRQHandler}, /* irq11 */

#############################################################

interrupt routine

##############################################################

INTERRUPT_HANDLER(EXTI_PORTD_IRQHandler, 6) // here is my input of 50 Hz on Pin D6

{

  

if(GPIO_ReadInputPin(GPIOD , GPIO_PIN_6))

{

timer1start = 1;

   }

}

INTERRUPT_HANDLER(TIM1_UPD_OVF_TRG_BRK_IRQHandler, 11)

{

 if (timer1start == 1)

 {  

TIM1_ClearITPendingBit(TIM1_IT_UPDATE);

flagfortimer = 1;

timer1start = 0;

 }

}

###############################################################

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Cristian Gyorgy
Senior III

Here you need to know your setup. Do you use an external zero crossing detector, or a pin through a R-C directly? What's your signal? What's the relay's switch time?

You need to figure out these things first, some basic theory, than you'll see things get quite simple...