cancel
Showing results for 
Search instead for 
Did you mean: 

STM8S105C4T6, inverting the UART2_TX signal

Kmax18
Senior II

I need an active high UART signal. Yes, the STM8S UART2_TX signal is active, but for hardware reasons I must invert the active low PCB output (UART2_TX). An easy solution would be a programmable STM8S feature to invert the signal. The reference manual does not list that option. Is that correct?

Thank you for your response.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Correct, unlike STM32, STM8 has no feature to invert UART TX.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Correct, unlike STM32, STM8 has no feature to invert UART TX.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you. Yes, that answers my question.

Great! I hope you find a way to invert the signal externally.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.