Skip to main content
janusz2
Associate
July 27, 2012
Question

stm8S003 constants at a fixed memory address

  • July 27, 2012
  • 4 replies
  • 2086 views
Posted on July 27, 2012 at 14:00

Hello

I'm trying place constants at fixed memory address according to this link 

http://www.cosmic-software.com/faq/faq3.php

My code is:

#pragma section const {sver}

const uint8_t SV_HIGH=1;

const uint8_t SV_MID=2;

const uint8_t SV_LOW=3;

#pragma section const{}

I added new segment into linker file:

+seg .sver -b 0x9f10

And linker returns:

#error clnk oprawa_v1.lkf:1 bad address (0x9f11) for zero page symbol _SV_MID

#error clnk oprawa_v1.lkf:1 bad address (0x9f12) for zero page symbol _SV_LOW

#error clnk oprawa_v1.lkf:1 bad address (0x9f10) for zero page symbol _SV_HIGH

Can Any One help?

    This topic has been closed for replies.

    4 replies

    janusz2
    janusz2Author
    Associate
    July 27, 2012
    Posted on July 27, 2012 at 15:45

    problem was in other file

    I by mistake badly externed const variable

    was:

    extern uint8_t SV_HIGH;

    should be:

    extern const uint8_t SV_HIGH;

    but whilst declaring segment you should use -k option becouse compiler optimizes your variable. for example:

    +seg .sver -b 0x9f10 -k

    carnett1
    Associate III
    August 1, 2012
    Posted on August 01, 2012 at 16:54

    You havew to go into stm8s.config and uncomment out define flash 1 and then use the routines in stm8s.flash I think that is the esame  in cosmic as in raisonance

    charles

    carnett1
    Associate III
    August 1, 2012
    Posted on August 01, 2012 at 16:58

    sorry it is stm8s_config.h

    charles

    carnett1
    Associate III
    August 1, 2012
    Posted on August 01, 2012 at 17:06

    again my ingers got ahead of my head stm8s.flash is really stm8s_flash.c

    charles