cancel
Showing results for 
Search instead for 
Did you mean: 

STM8S Printf retargeting doesn't like IAR Discard unused publics

Gordon Freeman
Associate

Hi all.

I'm trying to implement printf retargeting in my project, based on STM8S105 microcontroller.

I'm using IAR (3.10 & 2.20) and I'm utilizing printf retargeting example from ST. The problem is, if I try to compile the project with "Discard unused publics" option enabled, it stops working.

When I enable "Discard unused publics" option, I don't see any errors or warnings. I even decided to load original example from ST, and got the same results: with "Discard unused publics" option enabled retargeting stops working.

Can anyone give an Idea, what can cause such a problem?

Part of code, related to retargeting:

#ifdef _RAISONANCE_

#define PUTCHAR_PROTOTYPE int putchar (char c)

#define GETCHAR_PROTOTYPE int getchar (void)

#elif defined (_COSMIC_)

#define PUTCHAR_PROTOTYPE char putchar (char c)

#define GETCHAR_PROTOTYPE char getchar (void)

#else /* _IAR_ */

#define PUTCHAR_PROTOTYPE int extern putchar (int c)

#define GETCHAR_PROTOTYPE int getchar (void)

#endif /* _RAISONANCE_ */

/**

 * @brief Retargets the C library printf function to the UART.

 * @param c Character to send

 * @retval char Character sent

 */

PUTCHAR_PROTOTYPE

{

 /* Write a character to the UART */

 UART2_SendData8(c);

 /* Loop until the end of transmission */

 while (UART2_GetFlagStatus(UART2_FLAG_TXE) == RESET);

 return (c);

}

/**

 * @brief Retargets the C library scanf function to the USART.

 * @param None

 * @retval char Character to Read

 */

GETCHAR_PROTOTYPE

{

#ifdef _COSMIC_

 char c = 0;

#else

 int c = 0;

#endif

 /* Loop until the Read data register flag is SET */

 while (UART2_GetFlagStatus(UART2_FLAG_RXNE) == RESET);

  c = UART2_ReceiveData8();

 return (c);

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0