cancel
Showing results for 
Search instead for 
Did you mean: 

[STM8L001J3] Low-power STM8 MCU in 8-pin SO-8 package

Szymon PANECKI
Senior III
Posted on December 09, 2017 at 23:11

[STM8L001J3] Low-power STM8 MCU in 8-pin SO-8 package

Dear STM8 users,

ST has just officialy introduced to the market new low-cost, low-power 8-bit MCU from STM8 family. This device is named STM8L001J3 and its key new features are small pin count (8 pins) and tiny package (SO8N).

0690X00000608uMQAQ.png

After introducing in July first 8-pin STM8 MCU (

http://www.st.com/en/microcontrollers/stm8s001j3.html

), new

STM8L001J3 complements portofolio of 8-pin STM8 MCUs.

STM8L001J3 belongs to

STM8L Value line of ultra-low-power microcontrollers. It

offers the best price-to-performance ratio for cost-sensitive applications. With a similar core performance and peripheral set as the STM8L151/152 line, Value line has been optimized in terms of features and configurations to reach a budget price.

Some of important features of STM8L001J3:

  • Core and system
    • 2 internal clock sources (HSI 16MHz, LSI 38kHz)
    • Suply voltage range: from 1.8V to 3.6V
    • 6 I/Os
  • Timing peripherals
    • 8- and 16-bit general purpose timers
    • Auto-wakeup unit
    • Watchdog
  • Memories
    • 8k Flash
    • 1.5k RAM
    • 2k EEPROM
  • Conenctivity and debug
    • UART
    • SPI
    • I2C
    • Single Wire Interface Module (SWIM)
  • Analog
    • 2 comparators
0690X00000604BJQAY.jpg

You can start your design based on STM8L001J3 with free of charge development tools:

/external-link.jspa?url=http%3A%2F%2Fcosmicsoftware.com%2Fdownload_stm8_free.php

,

/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fen%2Fdevelopment-tools%2Fstm8cubemx.html

,

/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fen%2Fembedded-software%2Fstsw-stm8069.html

and

/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fen%2Fdevelopment-tools%2Fstvd-stm8.html

.

More information you can find on

http://www.st.com/content/st_com/en/products/microcontrollers/stm8-8-bit-mcus/stm8l-series/stm8l-value-line/stm8l001j3.html

.

Hardware getting started: minimum hardware needed for STM8L001J3 is decoupling circuitry (10uF + 100nF). It needs to be applied between VDD and VSS pins.

0690X00000604InQAI.jpg

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on May 08, 2018 at 08:17

Hello Fatih,

Thanks for your answer.

Good point regarding reference toSTM8L101. I confirmthat this description applies to STM8L001 as well. Sometimes documentation of Value Line devices is not so extensive and it is a good idea to refer to similar non Value Line device.

Good luck with evaluating STM8L001 MCU and in case of questions please feel free topost messages on the forum.

Regards

Szymon